This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TMS570LS0714: 2 TMS570 SPI Comunication problem (Master and Slave)

Part Number: TMS570LS0714


Tool/software: Starterware

Dear all,

I have a problem  with spi  for  two piece TMS570LS0714 communication.

The H/W  connect below:   one MASTER, one SLAVE.   SIMO-.>SIMO ,SOMI->SOMI, CLK->CLK, no others.

The program idea below:  Master send data[20] and receive data[20] in 1ms interrupt(HET interrupt, run well).Slave send data[20] and receive data[20] in 1ms interrupt(HET interrupt, run well).

But Master can send data (check register),not receive datas. Slave can  no neither.  Check Slave register , Flg register is 0x340 means OverRun. When  I  Clear 0x340 manually and I can see Slave  send and receive data just one data, and then FLG is 0x340 .  

I don't know how to slove the problem ,please help me. 

My code below:

Master:

void _InitSpi3(spiBASE_t *SpiInfo)
{
/* @b initialize @b SPI3 */
/** bring SPI out of reset */
SpiInfo->GCR0 = 1U;

/** SPI2 master mode and clock configuration */
SpiInfo->GCR1 = (1 << 1) /* CLOKMOD */
| 1; /* MASTER */

/** SPI3 enable pin configuration */
// spiREG3->ENAHIGHZ = 0; /* ENABLE HIGHZ *///lugh testtest

/** - Delays */
SpiInfo->DELAY = (4 << 24) /* C2TDELAY */
| (4 << 16) /* T2CDELAY */
| (0 << 8) /* T2EDELAY */
| 0; /* C2EDELAY */

/** - Data Format 0 */
SpiInfo->FMT0 = (63 << 24) /* wdelay */
| (0 << 23) /* parity Polarity */
| (0 << 22) /* parity enable */
| (0 << 21) /* wait on enable */
| (0 << 20) /* shift direction */
| (0 << 17) /* clock polarity */
| (0 << 16) /* clock phase */
| (79 << 8) /* baudrate prescale, 1M Hz *///lugh
// | (7 << 8) /* baudrate prescale, 10M Hz */
| 16; /* data word length */

/** - set interrupt levels */
SpiInfo->LVL = (0 << 9) /* TXINT */
| (0 << 8) /* RXINT */
| (0 << 6) /* OVRNINT */
| (0 << 4) /* BITERR */
| (0 << 3) /* DESYNC */
| (0 << 2) /* PARERR */
| (0 << 1) /* TIMEOUT */
| (0); /* DLENERR */

/** - clear any pending interrupts */
SpiInfo->FLG = 0xFFFFU;

/** - enable interrupts */
SpiInfo->INT0 = (0 << 9) /* TXINT */
| (0 << 8) /* RXINT */
| (0 << 6) /* OVRNINT */
| (0 << 4) /* BITERR */
| (0 << 3) /* DESYNC */
| (0 << 2) /* PARERR */
| (0 << 1) /* TIMEOUT */
| (0); /* DLENERR */

/** @b initialize @b SPI3 @b Port */

/** - SPI3 Port output values */
SpiInfo->PC3 = 1 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK */
| (0 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/** - SPI3 Port direction */
SpiInfo->PC1 = 1 /* SCS[0] */
| (0 << 8) /* ENA */
| (1 << 9) /* CLK */
| (1 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/** - SPI3 Port open drain enable */
SpiInfo->PC6 = 0 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK */
| (0 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/** - SPI3 Port pullup / pulldown selection */
SpiInfo->PC8 = 1 /* SCS[0] */
| (1 << 8) /* ENA */
| (1 << 9) /* CLK */
| (1 << 10) /* SIMO */
| (1 << 11); /* SOMI */

/** - SPI3 Port pullup / pulldown enable*/
SpiInfo->PC7 = 0 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK */
| (0 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/* SPI2 set all pins to functional */
SpiInfo->PC0 = 0 /* SCS[0] */
| (0 << 8) /* ENA */
| (1 << 9) /* CLK */
| (1 << 10) /* SIMO */
| (1 << 11); /* SOMI */

/** - Initialize TX and RX data buffer Status */
g_spiPacket_t[0].tx_data_status = SPI_READY;
g_spiPacket_t[0].rx_data_status = SPI_READY;

/*EmDataRegCfg for EM Config. */
EmDataRegCfg.CSNR = 1;
EmDataRegCfg.CS_HOLD = 1;
EmDataRegCfg.DFSEL = SPI_FMT_0;
EmDataRegCfg.WDEL = 1;

/** - Finally start SPI3 */
SpiInfo->GCR1 |=(uint32)((uint32)1U << 24U); /*SPI3 Enable */
}

uint32 Spi_TransmitAndReceiveData(spiBASE_t *spi,uint32 blocksize,
uint16 * srcbuff,uint16 * destbuff)
{
static uint16 Tx_Data;
uint16 RecvCnt = 0; /*Receive wait time count. */
static uint16 BuffHeaderFlag = 0;/* Receive header data finished flag. */

while(blocksize != 0U)
{
if((spi->FLG & 0x000000FFU) != 0U) /*Error occurs.*/
{
break;
}

Tx_Data = *srcbuff;

spi->DAT1 = (spi->DAT1 & 0xFFFF0000U) | ((uint32)Tx_Data);

srcbuff++;

while((spi->FLG & 0x00000100U) != 0x00000100U)
{
RecvCnt++;
// if(RecvCnt >= 500)
// {
// break;
// }//lugh
} /* Wait */

*destbuff = (uint16)(spi->BUF & 0xFFFFU);
if((blocksize == 20) && (*destbuff == 0xAAAA))//lugh
{
BuffHeaderFlag = 1;
}
if(BuffHeaderFlag == 1)
{
destbuff++;
}
blocksize--;
}
BuffHeaderFlag = 0;

return (spi->FLG & 0xFFU);
}

Slave:

void _InitSpi3(spiBASE_t *SpiInfo)
{
/* @b initialize @b SPI3 */
/** bring SPI out of reset */
SpiInfo->GCR0 = 1U;

/** SPI2 master mode and clock configuration */
SpiInfo->GCR1 = (0 << 1) /* CLOKMOD *///lugh
| 0; /* SLAVE */

/** SPI3 enable pin configuration */
// spiREG3->ENAHIGHZ = 0; /* ENABLE HIGHZ *///lugh testtest

/** - Delays */
SpiInfo->DELAY = (4 << 24) /* C2TDELAY */
| (4 << 16) /* T2CDELAY */
| (0 << 8) /* T2EDELAY */
| 0; /* C2EDELAY */

/** - Data Format 0 */
SpiInfo->FMT0 = (63 << 24) /* wdelay */
| (0 << 23) /* parity Polarity */
| (0 << 22) /* parity enable */
| (0 << 21) /* wait on enable */
| (0 << 20) /* shift direction */
| (0 << 17) /* clock polarity */
| (0 << 16) /* clock phase */
// | (79 << 8) /* baudrate prescale, 1M Hz */
| (7 << 8) /* baudrate prescale, 10M Hz */
| 16; /* data word length */

/** - set interrupt levels */
SpiInfo->LVL = (0 << 9) /* TXINT */
| (0 << 8) /* RXINT */
| (0 << 6) /* OVRNINT */
| (0 << 4) /* BITERR */
| (0 << 3) /* DESYNC */
| (0 << 2) /* PARERR */
| (0 << 1) /* TIMEOUT */
| (0); /* DLENERR */

/** - clear any pending interrupts */
SpiInfo->FLG = 0xFFFFU;

/** - enable interrupts */
SpiInfo->INT0 = (0 << 9) /* TXINT */
| (0 << 8) /* RXINT */
| (0 << 6) /* OVRNINT */
| (0 << 4) /* BITERR */
| (0 << 3) /* DESYNC */
| (0 << 2) /* PARERR */
| (0 << 1) /* TIMEOUT */
| (0); /* DLENERR */

/** @b initialize @b SPI3 @b Port */

/** - SPI3 Port output values */
SpiInfo->PC3 = 1 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK */
| (0 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/** - SPI3 Port direction */
SpiInfo->PC1 = 1 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK *///lugh
| (0 << 10) /* SIMO */
| (1 << 11); /* SOMI */

/** - SPI3 Port open drain enable */
SpiInfo->PC6 = 0 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK */
| (0 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/** - SPI3 Port pullup / pulldown selection */
SpiInfo->PC8 = 1 /* SCS[0] */
| (1 << 8) /* ENA */
| (1 << 9) /* CLK */
| (1 << 10) /* SIMO */
| (1 << 11); /* SOMI */

/** - SPI3 Port pullup / pulldown enable*/
SpiInfo->PC7 = 0 /* SCS[0] */
| (0 << 8) /* ENA */
| (0 << 9) /* CLK */
| (0 << 10) /* SIMO */
| (0 << 11); /* SOMI */

/* SPI2 set all pins to functional */
SpiInfo->PC0 = 0 /* SCS[0] *///lugh
| (0 << 8) /* ENA *///lugh
| (1 << 9) /* CLK */
| (1 << 10) /* SIMO */
| (1 << 11); /* SOMI */

/** - Initialize TX and RX data buffer Status */
g_spiPacket_t[0].tx_data_status = SPI_READY;
g_spiPacket_t[0].rx_data_status = SPI_READY;

/*EmDataRegCfg for EM Config. */
EmDataRegCfg.CSNR = 0;
EmDataRegCfg.CS_HOLD = 0;
EmDataRegCfg.DFSEL = SPI_FMT_0;
EmDataRegCfg.WDEL = 0;

/** - Finally start SPI3 */
SpiInfo->GCR1 |=(uint32)((uint32)1U << 24U); /*SPI3 Enable */
}

uint32 Spi_TransmitAndReceiveData(spiBASE_t *spi,uint32 blocksize,
uint16 * srcbuff,uint16 * destbuff)
{
static uint16 Tx_Data;
uint16 RecvCnt = 0; /*Receive wait time count. */
static uint16 BuffHeaderFlag = 0;/* Receive header data finished flag. */

while(blocksize != 0U)
{
if((spi->FLG & 0x000000FFU) != 0U) /*Error occurs.*/
{
break;
}

Tx_Data = *srcbuff;

spi->DAT1 = (spi->DAT1 & 0xFFFF0000U) | ((uint32)Tx_Data);

srcbuff++;

while((spi->FLG & 0x00000100U) != 0x00000100U)
{
RecvCnt++;
if(RecvCnt >= 500)
{
break;
}
} /* Wait */

*destbuff = (uint16)(spi->BUF & 0xFFFFU);
if((blocksize == 20) && (*destbuff == 0xAAAA))
{
BuffHeaderFlag = 1;
}
if(BuffHeaderFlag == 1)
{
destbuff++;
}
blocksize--;
}
BuffHeaderFlag = 0;

return (spi->FLG & 0xFFU);
}

  • Moving this thread to the Hercules forum.
  • Hello Arvin,

    You stated in your earlier description that you are using HET interrupts to trigger the transmit/receive, Correct? I don't see this in the example code you have provided. Are the Spi_TransmitReceiveData functions called within the HET interrupt? Given the code would appear to be sending 1 byte at a time, back to back, until 20 bytes are received, how do you gate the transmit of the second, third and subsequent bytes? i.e., I don't see the use of any CS or ENA pin to hold off transmit from the master until after data has been read by the slave. If you are not going to use any type of gating pin, you need to provide some delay in between bytes to insure there is sufficient time for the slave to reload the shift register and read out the received byte prior to the master initiating the next transfer. Generally speaking, you would need around 8 VCLK cycles between transmissions.