Other Parts Discussed in Thread: LMFLASHPROGRAMMER, TM4C1294NCPDT, SEGGER, UNIFLASH
Greetings,
This is my first time to proceed from evaluation kit into the design implementation. I would like to minimize the footprint, so I will not put any USB interface or JTAG(UART) if it is possible. Of course I have been investigating the Manual for TM4C Bootloader API and LMFLASHPROGRAMMER, and it seems it is possible for me to use Ethernet as programming port.
I will use TM4C1294NCPDT as my MCU and I read that "Internal ROM loaded with TivaWare™ for C Series software".
The question that I have are:
1)If I buy the chip from Digikey/Mouser, does a bootloader come with it?
2)If #1) is Yes, can I use the LMFLASHPROGRAMMER to download the .bin from CCS and the device will have the same function as my evaluation board?
3)if #1) is No, how can I be able to initially program it?
4) What are the tools that I needed to download the program, if I am using the JTAG(Uart) -- I can possibly buy the USB->TTL3.3V or using any recommendation hardware that are easy to use. But, I believe that if TM4C comes with bootloader in it, I can just possibly use Ethernet to initialize the program files.
5) Do you have any suggestion so that I can easily mass produce this MCU (around 100) by myself?
Thanks,
Yo Shua