Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: TM4C123GH6PM, TM4C1294NCPDT, TM4C123AH6PM
When compiling a TivaWare project, it is necessary to specify the part using a project-level predefined preprocessor symbol, such as (in my case) PART_TM4C123GH6PM.
But to use the ROM_ functions defined in rom.h and rom_map.h, a 2nd define is needed, of the form TARGET_IS_TM4C12x_Rxx. There are a variety of possibilities: TARGET_IS_TM4C123_RA1, TARGET_IS_TM4C123_RA3, TARGET_IS_TM4C123_RB1, etc.
I have two questions about this:
1. Since I have #defined PART_TM4C123GH6PM (by means of the project settings), why aren't the TivaWare headers automatically defining the correct TARGET_IS_ symbol? As in:
#if defined (PART_TM4C123GH6PM)
#define THE_CORRECT_TARGET_IS_DEFINE_HERE
#endif
2. Since TivaWare is not doing this automatically, what is the correct TARGET_IS_ define to use for PART_TM4C123GH6PM?
I am using TivaWare 2.1.4.178.