Part Number: EK-TM4C123GXL
I have a confusion about oversampling.
According to Wikipedia, oversampling is the process of sampling a signal with a sampling frequency significantly higher than the Nyquist rate. How I understand is that, oversampling is sampling at a much higher sampling rate, compared to single conversion.
However, I found this information on the driver user guide, "Hardware oversampling of the ADC data is available for improved accuracy. An oversampling factor of 2x, 4x, 8x, 16x, 32x, or 64x is supported, but reduces the throughput of the ADC by a corresponding factor. Hardware oversampling is applied uniformly across all sample sequencers".
So is oversampling's sampling rate/throughput higher or lower than single's?