Part Number: TM4C123GH6PM
I am trying to implement an SSI EOT interrupt and I'm not having much success. I started with some sample code that did not have interrupts enabled and had a SysCtlDelay() after the write to hold the *CS gpio line low until the last bit was clocked out. This works ok, but now I'm trying to make the code more efficient and faster. So, I'd like to instead wait on the interrupt to come in and then drop the chip select. Interrupts do occur, but I'm expecting just the SSI_TXFF interrupt and I get everything but that one. Per the datasheet, I set the EOT bit in the SSI1_CR1R register. What I'm not sure about is the correct placement of this call? Should it be made prior to the Interrupts being enabled? (where I do it now.)
Here is my SSI initialization code:
void SpiInit_SSI1(void) {
// The SSI1 peripheral must be enabled for use.
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
// For the TM4C123G, SSI0 is used with PortA[5:2].
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
// Configure the pin muxing for SSI0 functions on port A2, A3, A4, and A5.
ROM_GPIOPinConfigure(GPIO_PD0_SSI1CLK); // Configure PA2 for the clock
ROM_GPIOPinConfigure(GPIO_PD2_SSI1RX);
ROM_GPIOPinConfigure(GPIO_PD3_SSI1TX); // Configure PA5 for the Master Transmit
// Configure the GPIO settings for the SSI pins. This function also gives
// control of these pins to the SSI hardware. Consult the data sheet to
// see which functions are allocated per pin.
// The pins are assigned as follows:
// PA5 - SSI0Tx
// PA4 - SSI0Rx
// PA3 - SSI0Fss - Not Used
// PA2 - SSI0CLK
ROM_GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_2 | GPIO_PIN_3);
// Configure and enable the SSI port for SPI master mode. Use SSI1,
// system clock supply, idle clock level low and active low clock in
// freescale SPI mode, master mode, 1MHz SSI frequency, and 8-bit data.
// For SPI mode, you can set the polarity of the SSI clock when the SSI
// unit is idle. You can also configure what clock edge you want to
// capture data on. Please reference the datasheet for more information on
// the different SPI modes.
ROM_SSIConfigSetExpClk(SSI1_BASE, 80000000, SSI_FRF_MOTO_MODE_0,
SSI_MODE_MASTER, 2000000, 16);
SSIIntDisable(SSI1_BASE, 0x0F);
SSI1_CR1_R |= 0x00000010;
SSIIntEnable(SSI1_BASE, SSI_TXFF);
SSIIntRegister(SSI1_BASE, &Ssi1IntHandler);
// Enable the SSI0 module.
ROM_SSIEnable(SSI1_BASE);
uint32_t pui32DataRx[2];
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
while(ROM_SSIDataGetNonBlocking(SSI1_BASE, &pui32DataRx[0])){ }
}