Part Number: TIDM-TM4C129XNFC
Other Parts Discussed in Thread: CC31XXEMUBOOST, CC3100BOOST, EK-TM4C1294XL, UNIFLASH, CC3100
Tool/software: TI-RTOS
Hi,
I need to read ISO14443A/B Type 4 NFC cards, so I’m using:
- This setup: www.ti.com/.../TIDM-TM4C129XNFC
- These instructions: www.ti.com/.../tiduag2a.pdf
To support this software I have the following hardware, which includes two options for NFC (7970A & RF430).
- EK-TM4C1294XL-TM4C1294 Connected LaunchPad
- CC3100BOOST-SimpleLink Wi-Fi CC3100 wireless network processor BoosterPack plug-in module
- CC31XXEMUBOOST-Advanced Emulation BoosterPack for SimpleLink Wi-Fi CC3100 BoosterPack plug-in module
- DLP-7970ABP-TRF7970A NFC BoosterPack
- DLP-RF430BP-RF430CL330H NFC T4BT Platform BoosterPack
My questions are:
- Is the CC31XXEMUBOOST only needed to flash / copy files to the CC3100BOOST and therefore should NOT be connected with running the NFC software?
- Page 17 of tiduag2a.pdf specifically asks for RTOS 2.14. Is RTOS 2.16 ok to use instead?
- What Target Config "Tiva C" card should I be using with a EK-TM4C1294XL? Is the Tiva TM4C129NCPDT ok since the EK-TM4C1294XL is not listed?
- I get the errors shown in the screenshot when trying to build the NFC sample code, what should I do to get it working?
Thanks in advance for your help!
Cheers,
Tim