Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN
*Safety feature "EMF3".
I using TMS570LS3137, and reading Safety Manual(SPNU511D).
I using HAL_CoGen (ver.04.05.01).
I have doubts about the source code generated from HAL_CoGen.
I will talk about the emif module as an example.
In the generated code, there is emifGetConfigValue ().
Here, I am aware that we are comparing the initial value and the current value.
* Initial value setting to the register is implemented by emif_ASYNC1Init () etc.
It seems that the value set as the initial value and the define value treated as the initial value by emifGetConfigValue () are different.
Does it always make a failure judgment with the safety feature "EMF 3"?
Is there a problem with the HAL_CoGen tool?
Or is there a mistake in my perception?