This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: HTTPCli_connect doesn't connect with static IP (error code 102), but works with DHCP

Expert 2730 points

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

As the topic says I have problem with HTTPCli_connect when using static IP, but if DHCP is defined it works. I have checked the communication with the Wireshark and if I use static ip it doesn't even send anything with the HTTPCli_connect. HTTPCli_initSockAddr works perfectly, means it gets the IP address from hostname from the manual defined DNS server. Below the code.

TI-RTOS: 2.16.1.14

XDCTools: 3.32.0.06

NDK: 2.25.00.09

Ip.autoIp = true; is always configured and will be turned off later when configuring the static IP.
/* ================ NDK configuration ================ */
var Ndk		= xdc.loadPackage('ti.ndk.config');
var Global	= xdc.useModule('ti.ndk.config.Global');
var Ip		= xdc.useModule('ti.ndk.config.Ip');
var Tcp		= xdc.useModule('ti.ndk.config.Tcp');

Global.IPv6 = false;
Global.stackLibType = Global.MIN;
Global.networkOpenHook = "&TcpHooks_vNetOpenHook";
Global.networkIPAddrHook = "&TcpHooks_vIPAddrHook";

/* automatically call fdOpen/CloseSession for our sockets Task */
Global.autoOpenCloseFD = true;

Global.pktNumFrameBufs = 10;
Global.memRawPageCount = 6;
Global.ndkThreadStackSize = 1536;
Global.lowTaskStackSize = 1024;
Global.normTaskStackSize = 1024;
Global.highTaskStackSize = 1024;

Tcp.transmitBufSize = 1024;
Tcp.receiveBufSize = 1024;

Ip.autoIp = true;

/* ================ HTTP configuration ================ */
var Http = xdc.useModule('ti.net.http.Http');
Http.networkStack = Http.NDK;
void TcpHooks_vNetOpenHook(void)
{
    IPN IPTmp;
    CI_IPNET NA;
    HANDLE hCfgIpAddr;
    HANDLE hCfg;
    int ret;

    bIPAddressChanged();

    hCfg = CfgGetDefault();
    if (!hCfg)
    {
        System_abort("Couldn't fetch handle\n");
    }

    ret = CfgGetEntryCnt(hCfg, CFGTAG_IPNET, 1);
    System_printf("Static IP count: %d\n", ret);

    /* get the current static IP entry */
    if (CfgGetEntry(hCfg, CFGTAG_IPNET, 1, 1, &hCfgIpAddr))
    {
        /* remove the current static IP entry */
        if (CfgRemoveEntry(hCfg, hCfgIpAddr) < 0)
        {
            System_abort("Couldn't remove static IP entry\n");
        }
    }
    else
    {
        System_printf("Couldn't get static IP entry\n");
    }

    // Manually add the DNS server when specified
    IPTmp = inet_addr(strDnsAddr);
    if (IPTmp)
    {
        if (CfgAddEntry(hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_DOMAINNAMESERVER,
                        0, sizeof(IPTmp), (UINT8 *)&IPTmp, 0 ) < 0)
        {
            System_abort("Couldn't add static IP entry\n");
        }

    }
    else
    {
        System_printf("Couldn't add DNS IP\n");
    }

    /* Setup manual IP address */
    bzero(&NA, sizeof(NA));
    NA.IPAddr  = inet_addr(strIpAddr);
    NA.IPMask  = inet_addr(strIpMask);
    strcpy(NA.Domain, "own.com");
    NA.NetType = 0;

    /* add a new static IP entry */
    if (CfgAddEntry(hCfg, CFGTAG_IPNET, 1, 0,
                    sizeof(CI_IPNET), (UINT8 *)&NA, 0) < 0)
    {
        System_abort("Couldn't add static IP entry\n");
    }
}
void TcpHooks_vIPAddrHook(IPN IPAddr, uint IfIdx, uint fAdd)
{
    IPN IPTmp;
    CI_IPNET NA;
    HANDLE hCfg;
    int rc = 0;
    char IPString[16];

    hCfg = CfgGetDefault();

    /* Initialize the IP Address block. */
    bzero(&NA, sizeof(CI_IPNET));

    if (fAdd)
    {
        System_printf("networkIPAddrHook: Network Added\n");
        Semaphore_post(semaphoreNdkStack);
    }
    else
    {
        System_printf("networkIPAddrHook: Network Removed\n");
    }

    IPTmp = ntohl(IPAddr);
    System_printf("networkIPAddrHook:\tIf-%d:%d.%d.%d.%d\n", IfIdx,
                  (UINT8)(IPTmp>>24)&0xFF, (UINT8)(IPTmp>>16)&0xFF,
                  (UINT8)(IPTmp>>8)&0xFF, (UINT8)IPTmp&0xFF);

    /* Print the IP address information only if one is present. */
    if (CfgGetImmediate(hCfg, CFGTAG_IPNET, 1, 1, sizeof(NA), (UINT8 *)&NA) == sizeof(NA))
    {
        /* Yes the device was configured and we got the IP address/Mask */
        NtIPN2Str (NA.IPAddr, IPString);
        System_printf("IP Address: %s\n", IPString);
        NtIPN2Str (NA.IPMask, IPString);
        System_printf("IP Subnet Mask: %s\n", IPString);
    }
    else
    {
        System_printf("IP Address & SUBNET MASK NOT AVAILABLE\n");
    }

    rc = CfgGetImmediate(hCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_DOMAINNAMESERVER,
                         1, 4, (UINT8 *)&IPTmp );
    if (rc == 4)
    {
        IPTmp = ntohl(IPTmp);
        System_printf("networkIPAddrHook:\tIf-%d: DNS = %d.%d.%d.%d\n", IfIdx,
                      (UINT8)(IPTmp>>24)&0xFF, (UINT8)(IPTmp>>16)&0xFF,
                      (UINT8)(IPTmp>>8)&0xFF, (UINT8)IPTmp&0xFF);
    }
    else
    {
        System_printf("networkIPAddrHook: DNS IP Fetch Failed!!\n");
    }
}
void Cloud_vWork(void)
{
    struct sockaddr_in addr;
    char cContentLength[5];
    int count;
    int ret;
    int dataSize = 64;
    int offset;

    HTTPCli_Struct cli;
    HTTPCli_Field fields[2] =
    {
     { HTTPStd_FIELD_NAME_HOST, HOSTNAME },
     { NULL, NULL }
    };

    Semaphore_pend(semaphoreNdkStack, 10000); // wait 10 s for the stack to initialize and get ip

    fdOpenSession(Task_self()); // open the NDK file descriptor session for this thread

    
        HTTPCli_construct(&cli);
        HTTPCli_setRequestFields(&cli, fields);

        while (1)
        {
            System_printf("Sending a HTTP PUT request to '%s'\n", HOSTNAME);

            ret = HTTPCli_initSockAddr((struct sockaddr *)&addr, HOSTNAME, 0);
            if (ret < 0) {
                printError("httpTask: address resolution failed", ret);
                continue;
            }

            ret = HTTPCli_connect(&cli, (struct sockaddr *)&addr, 0, NULL);
            if (ret < 0) {
                printError("httpTask: connect failed", ret);
                continue;
            }
            Task_sleep(FIVE_MINUTES);
        }
}

Everything works if I comment everything out from the TcpHooks_vNetOpenHook. I have followed with the debugger from the HTTPCli_connect, which is not easy from optimized code, to place where it just can't find the route to the destination. What could be the reason?

BR

JHi 

  • Hier the routing tables for DHCP (192.168.2.107) and for the static IP (192.168.2.111). The static IP is also free in our network so the reason can't be address collision

    Address          Subnet Mask      Flags   Gateway
    ---------------  ---------------  ------  -----------------
    
    192.168.2.0      255.255.255.0    U   C   if-1
    192.168.2.107    255.255.255.255  U H  L  local (if-1)
    
    192.168.2.0      255.255.255.0    U   C   if-1
    192.168.2.111    255.255.255.255  U H  L  local (if-1)

  • Problem solved. I had forgotten to configure gateway:

    bzero( &RT, sizeof(RT) );
        RT.IPDestAddr = 0;
        RT.IPDestMask = 0;
        RT.IPGateAddr = inet_addr(strIpGateway);
        // Add the route
        if (CfgAddEntry( hCfg, CFGTAG_ROUTE, 0, 0,
                         sizeof(CI_ROUTE), (UINT8 *)&RT, 0) < 0)
        {
            System_abort("Couldn't add route entry\n");
        }

    JHi