Other Parts Discussed in Thread: TPS65381-Q1
Team,
I'm posting this on behalf of my customer:
"We are using the RM48 processor in a SIL application, we need to implement voltage supervision. I was working on the undervoltage supervision for the core voltage and I implemented it with a device which combines a watchdog with an undervoltage monitor. This turns out to be quite tricky since the nominal core voltage of the RM48 and the lower limit of the core voltage range of the RM48 are extremely close, especially if you consider also the regulator’s accuracy.
Can you tell me if the 1.14V is the very lowest absolute threshold for the undervoltage monitor on the RM48 for functional safety applications?
Or in other words; how critical is it for SIL when the undervoltage has a minimum warning level at 1.10V instead of 1.14?"
Thanks,
Tom