This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294NCPDT: Can I use the firmware of XDS 110 for my application scheduled to be mass-produced?

Part Number: TM4C1294NCPDT

Tool/software: Code Composer Studio

Hello.

I have a question.

Can I use the firmware of XDS 110 for my application scheduled to be mass-produced?

I would like to create an educational board that allows users to debug MSP432P401M with CMSIS DAP using TM4C1294 NCPDT

I think that XDS110 can be used as CMSIS DAP, so I would like to write the binary file in following directory to TM4C1294NCPDT.

C:\ti\ccsv7\ccs_base\common\uscif\xds110

Is it possible to use the above files for mass production?

Regards,

uchida-k