Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hello,
I am using the Hercules RM48L952 development board. I am trying to obtain data using a SPI interface (as a master) and send data using the Ethernet interface.
I have tested SPI1 and SPI2 (I have not tried SPI3 or SPI5 yet), but I can only send SPI transmissions using these peripherals when the Ethernet switch on the board (on a set of switches labeled S2) is turned off. This implies there are lines for SPI and Ethernet that are muxed on this board, but I have poured through the datasheets and looked at the Halcogen PINMUX tab, and I can't see anything regarding this.
Is it possible to use SPI and Ethernet on this board for the same application?
John