Part Number: TM4C1294NCPDT
Hi, I'm trying to use the slave transmit FIFO so I can send data to another logging device.
I'm having problems with no data being transmitted on the bus even though the FIFO is full. I think it's a problem with my setup commands.
Slightly Abriged Code:
ulI2CController=I2C0_BASE;
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_I2C0)){}
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOB)){}
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
I2CSlaveInit(I2C0_BASE, 42);
I2CSlaveFIFOEnable(I2C0_BASE,I2C_SLAVE_TX_FIFO_ENABLE);
I2CTxFIFOConfigSet(I2C0_BASE,I2C_FIFO_CFG_TX_SLAVE);
while(1)
{
I2CFIFODataPut(I2C0_BASE, 5);
}