Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Dear sir / madam,
I am trying to obtain as much free GPIO as possible for a project, using the RM48x 337 BGA (ZWT)
Realistically I need ate least 116 GPIO pins.
I'm using the peripherals: 3-CAN, 1-I2C, and USB HOST and DEVICE.
The pins spare I am unsure of are External Memory Interface (EMIF) and the A2D pins.
Im guessing the EMIF could be used, however some of these pins are taken when configuring the RAM trace port (RTP) as GPIO.
The A2D im guessing cannot be used for GPIO?
Any ideas, is there a way of using the EMIF to get IO, i.e. could outputs be obtained by using data latch chips and chip selects/data lines form the micro?
Thanks
Brendan Johnson