Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: TM4C123GH6PM,
Hello Forum,
I am working with EK-TM4C123GXL Launchpad with TM4C123GH6PM MCU, Keil uVision5 IDE, and LM Flash Programmer - Build 1613. I had this whole development chain working perfectly and was going good. But some days when I fire up the system my PC does not see the Stellaris Virtual COM Port, nor the Stellaris ICDI Debug Interface - i.e. these are NOT listed in the Hardware list of my PC. If I restart PC, which powers down and powers up again the EK-TM4C123GXL Launchpad via USB port, sometimes then the Stellaris Virtual COM Port, and the Stellaris ICDI Debug Interface are listed in the Hardware list of my PC. I can then proceed to open up Keil uVison5 and try programming my Launchpad via the Load button at top of IDE screen. LM Flash Programmer opens up, but when I try Program, the Programming often fails after 17%, 25% etc. The LM Flash Programmer just not functioning perfectly. Sometimes Programming does complete to 100% and Verify succeeds but the loaded program will not run. I have searched and read on the Forums regarding problems related to mine and similar to mine. It makes somewhat torturous and tiresome reading.
I am going to bin my Stellaris IDCE Debug Interface. Could anyone please suggest a recommend a better not too expensive Programming/Debugging method for the EK-TM4C123GXL Launchpad?, please.
Yours Sincerely,
John O'Connor