Part Number: LAUNCHXL2-RM57L
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello,
I am working on a project based on "HALCoGen Ethernet Driver and lwIP" example project. Everything is working on debug mode but when i try to power on board without connected computer,Program get stuck.
If a reset board, working correct.I try to power on external 5v jack then connect usb to pc. Board print out "." character for about 5 minutes then boot.if i reset board with reset buton, board boot correctly.
Thanks.
/** @file HL_sys_main.c
* @brief Application main file
* @date 20.May.2014
* @version 04.00.00
*
* This file contains an empty main function,
* which can be used for the application.
*/
/* (c) Texas Instruments 2009-2013, All rights reserved. */
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
#include "HL_system.h"
/* USER CODE BEGIN (1) */
extern void EMAC_LwIP_Main (uint8_t * emacAddress);
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
/* USER CODE END */
uint8 emacAddress[6U] = {0x00U, 0x08U, 0xEEU, 0x03U, 0xA6U, 0x6CU};
uint32 emacPhyAddress = 1U;
uint8 ip_addr[4];
void main(void)
{
/* USER CODE BEGIN (3) */
sciInit();
EMAC_LwIP_Main(emacAddress);
/* USER CODE END */
}
/* USER CODE BEGIN (4) */
/* USER CODE END */