Part Number: TM4C123GH6PM
In my application I am facing a data loss. So I tried to create a FIFO using 7 message objects.
But the data are receiving only in the lowest object. Given below is my code
void CAN_Config(void)
{
// enable the PORT-E for CAN TX & RX
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE); // enable the PORTE
GPIOPinConfigure(GPIO_PE4_CAN0RX); // configure the PE4 for CAN receiving function
GPIOPinConfigure(GPIO_PE5_CAN0TX); // configure the PE5 for CAN transmitting function
GPIOPinTypeCAN(GPIO_PORTE_BASE, GPIO_PIN_4 | GPIO_PIN_5); // enable the pin types for CAN
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
// initialize the CAN0
CANInit(CAN0_BASE);
IntEnable(INT_CAN0);
// enable the interrupt on the CAN peripheral
CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
CANEnable(CAN0_BASE);
}
*****************************************************************************
void can_info(uint32_t baudRate,uint8_t samplingPoint)
{
// assigning the CAN bit timing structure values for CAN transmit and receive
// ToDo:Currently bit_time_q is constant in all baudRates;Need to validate it.
if (baudRate == 1000)
{
GetBittime.ui32SyncPropPhase1Seg=15;
GetBittime.ui32Phase2Seg=4;
GetBittime.ui32SJW=3;
GetBittime.ui32QuantumPrescaler=4;
}
else
{
// ToDo:baudrate is not supported;Handle this as an error.
}
// set that assigning values to that CAN
CANBitTimingSet(CAN0_BASE, &GetBittime);
// assign the CAN message object structure members for receving the data
sMsgObjectRx.ui32MsgIDMask = 0Xffff;
// The first 5 message objects have the MSG_OBJ_FIFO set to indicate
// that they are part of a FIFO.
sMsgObjectRx.ui32Flags = (MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER | MSG_OBJ_EXTENDED_ID | MSG_OBJ_FIFO );
sMsgObjectRx.pui8MsgData = pui8MsgData;
sMsgObjectRx.ui32MsgLen = 8;
// The first three message objects have the MSG_OBJ_FIFO set to indicate
// that they are part of a FIFO.
CANMessageSet(CAN0_BASE, 2, &sMsgObjectRx, MSG_OBJ_TYPE_RX);
CANMessageSet(CAN0_BASE, 3, &sMsgObjectRx, MSG_OBJ_TYPE_RX);
CANMessageSet(CAN0_BASE, 4, &sMsgObjectRx, MSG_OBJ_TYPE_RX);
CANMessageSet(CAN0_BASE, 5, &sMsgObjectRx, MSG_OBJ_TYPE_RX);
CANMessageSet(CAN0_BASE, 6, &sMsgObjectRx, MSG_OBJ_TYPE_RX);
// Last message object does not have the MSG_OBJ_FIFO set to indicate that
// this is the last message.
sMsgObjectRx.ui32Flags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER;
CANMessageSet(CAN0_BASE, 7, &sMsgObjectRx, MSG_OBJ_TYPE_RX);
}
void CANIntHandler(void)
{
uint32_t ui32Status;
// Read the CAN interrupt status to find the cause of the interrupt
ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
// If the cause is a controller status interrupt, then get the status
if(ui32Status == CAN_INT_INTID_STATUS)
{
// Read the controller status
ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
// set the error flag
g_bErrFlag = 1;
}
// Check if the cause is message object 1, which what we are using for
// sending messages.
else if(ui32Status == 1)
{
//-----------Transmit Interrupt-----------//
// If this condition is true, then the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
CANIntClear(CAN0_BASE, 1);
g_ui32MsgCount_Tx++;
// clear the error flag
g_bErrFlag = 0;
}
//-------------Receive Interrupt-----------//
// If this condition is true, then the RX interrupt occurred on
// message object 2, and the message RX is complete.
else if(ui32Status == 2)
{
g_ui32MsgCount_Rx++;
CANMessageGet(CAN0_BASE, 2, &sMsgObjectRx, 1);
// clear the error flag
g_bErrFlag = 0;
}
else if(ui32Status == 3)
{
g_ui32MsgCount3_Rx++;
CANMessageGet(CAN0_BASE, 3, &sMsgObjectRx, 1);
// clear the error flag
g_bErrFlag = 0;
}
else if(ui32Status == 4)
{
g_ui32MsgCount4_Rx++;
CANMessageGet(CAN0_BASE, 4, &sMsgObjectRx, 1);
// clear the error flag
g_bErrFlag = 0;
}
else if(ui32Status == 5)
{
g_ui32MsgCount5_Rx++;
CANMessageGet(CAN0_BASE, 5, &sMsgObjectRx, 1);
// clear the error flag
g_bErrFlag = 0;
}
else if(ui32Status == 6)
{
g_ui32MsgCount6_Rx++;
CANMessageGet(CAN0_BASE, 6, &sMsgObjectRx, 1);
// clear the error flag
g_bErrFlag = 0;
}
else if(ui32Status == 7)
{
g_ui32MsgCount7_Rx++;
CANMessageGet(CAN0_BASE, 7, &sMsgObjectRx, 1);
// clear the error flag
g_bErrFlag = 0;
}
}