Part Number: EK-TM4C1294XL
CC7.2, TivaWare_C_Series-2.1.4.178.
I'm trying to run the uart_echo example. I have the EK set up for the uart_echo demo just as
Lab 10 says.
When I run the example, nothing happens. I tried pressing the reset button, I don't see
anything prompting me to enter text.
I have PuTTY 0.70 installed on windows 10. I am unable to open a PuTTY terminal window.
I have the correct COM serial port, the baud rate set to 115200, flow control OFF. These settings
are consistent with the Stellaris virtual serial COM port. Why won't the terminal open?
Thanks,
Priya