Part Number: TMS570LS1224
Other Parts Discussed in Thread: LAUNCHXL2-TMS57012, TMS570LC4357, , HALCOGEN
Hi everyone,
I am trying to setup a MibSPI connection between a TMS570LS1224 (LAUNCHXL2-TMS57012) and a TMS570LC4357 (LAUNCHXL2-TMS570LC43).
I plugged the launchpads using booster pack, so I am using MibSPI3.
The two uP have different clocks, so I set 2 different baudrate (15MHz for the 4357 and 16Mhz for the 1224). I am using a single transfer group of 16 words triggered by chip select 1 (CS0 is not mapped to the booster pack). I use 4 pin mode
I see that the slave device (1224) start to reply only after 350 ms, and I can't realize why. The startup call exactly the same functions in the same order for both. I tried also to set a breakpoin at the end of the slave a configuration and starting the master at this time, but with no good results.
After this time the communication is going perfectly, I see no errors.
Can anyone give me some help? Let me know if you need more informations!
Thank you,
Arianna