Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Hello,
I'm working on developing a bootloader on Hercurles HDK RM48L952:
- The bootloader is the TI Bootloader Ethernet
- The user application is based on Micrium OS uCOS-III.
The initialization of the bootloader calls the service "_coreEnableIrqVicOffset_" to enable IRQ handling via VIC Controller. The initialization of the user application doesn't call the service "_coreEnableIrqVicOffset_", as this mode is not compatible with uCOS-III.
But when the user application is initialized (sys_startup.c generated by HALCoGen), the bit VE in the register System Control Register (SCTLR) is not reset to 0. So I have written a service "_coreDisableIrqVicOffset_" to force the reset of the bit.
I'm not sure it's the right way to do that. Is there any function, generated by HALCoGen, to reset this register ?
Best regards
Pierre