Part Number: TM4C123GH6PM
Tool/software: TI-RTOS
Hi forum,
I am a little confused and just wondering at the moment: is it possible to use multiple UARTs with the TI RTOS framework on a comfortable way? On my own hardware I am using the given UART example with a console and a terminal program. Using the SysCallback functionality it works flawless with scanf and system_printf. In a next step I want to use another UART connected to a bluetooth IC. Is there a possiblity to share(?) the SysCallback interface or create another? I could use the interrupt linked to the UART2 device, but this way I have to handle the data myself. In the best case I would have something like scanf(UART0,...) and a system_printf(UART0,...).
Thanks in advance.