Part Number: LAUNCHXL2-TMS57012
Other Parts Discussed in Thread: HALCOGEN
i want to start conversion of ADC(ambient_lightsensor[AD1IN_6]) with external input by setting the voltage of one of GIO pins to high from almost zero (3.3v or 5v) . i configure the halcogen as below :
drivers : GIO / SCI2LIN (for serial transmission of sampled voltage) / ADC1
GIO : port b bit 0 : set to rising edge and enable connection to VIM.
PINMUX : enable GIOB and AD1EVT (may be not needed at all )
ADC1 Group Event : ADC1 Group trigger source GIOB0 on default and Trigger edge to rising edge. / enable pin 6 for voltage sampling of ambient light sensor(on this very board) .
and this is my code in sys_main.c
int main(void)
{
//initializing SCI module
sciInit() ;
//initializing ADC module
adcInit() ;
//initializing GIO module
gioInit() ;
uint32 grp = 1 ;
adcData_t adc_dat ;
adcData_t * pr_adc_dat = &adc_dat ;
uint32 num_digit = 0 ;
char ch[10] ;
char* pr_ch = &ch[0] ;
//fist comment //
sciSend(scilinREG , 24 , "Ambient Light Viewer :\r\n") ;
while(1){
while(adcIsConversionComplete(adcREG1 , 1) == 0) ;
adcGetData(adcREG1 , 1 , pr_adc_dat ) ;
num_digit = ltoa(pr_adc_dat->value, pr_ch) ;
sciSend(scilinREG , 2 , "v:" ) ;
sciSend(scilinREG , num_digit , pr_ch ) ;
sciSend(scilinREG , 2 , "\r\n") ;
//after each iteration set the isconversioncomplete to false ...
//wait until again GIOB0 voltage set to HIGH (3.3 or 5) ...
adcREG1->GxINTFLG[grp] = (uint32) 0U ;
}
return 0;
}
im not examining the SCI module because it works for the first comment ( refer to code) ...
i have no idea why when i set GIOB_0 to HIGH logical value externally the conversion is not begin( note that i leave the GIOB_0 pin with it's default input direction).