Part Number: RM46L852
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello,
I have configured a TG of 4 buffers that is doing what it should (send 1 byte as command and receive 7 bytes of data to/from an acc sensor) when it is triggered via SW:
while(1) {
delay(15); // faster than the sensor's data rate
mibspiREG5->TGCTRL[3] = (3*TG_STARTBUF) + TRIG_SW + ONESHOT + (uint32)TGENA;
while ((mibspiREG5->TGINTFLG & 1<<(16+3)) == 0) ; // wait for transfer-completed flag
echoAccDataViaSCI(); // got it
}
The sensor is configured to emit an interrupt on new data. With the readout still timed using a delay loop, I see the signal rising on new data and falling on readout as expected. The following code lets the MibSPI use it:
gioREG->GCR0 = 1; // GIO module out of reset gioPORTA->PULDIS = 1<<7; // INT1 pin of acc sensor is push-pull by default mibspiREG5->TGCTRL[3] = (3*TG_STARTBUF) + TRIG_GIOA7 + TRIG_RISING + (uint32)TGENA;
Works well, tested by a modified loop body:
while(1) {
while ((mibspiREG5->TGINTFLG & 1<<(16+3)) == 0) ; // wait for transfer-completed flag
mibspiREG5->TGINTFLG = 1<<(16+3); // clear that flag
echoAccDataViaSCI();
}
Then, instead of the loop body, I registered the following ISR in sys_vim.c (at both levels, idx-1 = 53, 56):
int test = 13;
#pragma INTERRUPT(mibSPI5ISR, IRQ)
void mibSPI5ISR(void) {
mibspiREG5->TGINTFLG = 0xffffffff; // clear flags
test = 42;
// basic statistics on acc-sensor datagrams
}
and enabled the interrupt:
mibspiREG5->TGITENST = 1<<(16+3); _enable_interrupt_();
but test (at file scope) keeps at 13. What is missing?