Part Number: EK-TM4C123GXL
Hi,
I copied usb_host_keyboard code from Dk-tm4c123g and customise for EK-TM4C123GXL. But not sense keyboard. What is problem. My code is at following. And I add functions to startup file. extern void SysTickIntHandler(void); extern void USB0OTGModeIntHandler(void);
Note: We give Vbus 5V directly.
//*****************************************************************************
//
// usb_host_keyboard.c - main application code for the host keyboard example.
//
// Copyright (c) 2012-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.4.178 of the DK-TM4C123G Firmware Package.
//
//*****************************************************************************
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "driverlib/rom.h"
#include "driverlib/uart.h"
#include "usblib/usblib.h"
#include "usblib/usbhid.h"
#include "usblib/host/usbhost.h"
#include "usblib/host/usbhhid.h"
#include "usblib/host/usbhhidkeyboard.h"
#include "utils/uartstdio.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>USB HID Keyboard Host (usb_host_keyboard)</h1>
//!
//! This example application demonstrates how to support a USB keyboard
//! attached to the evaluation kit board. The display will show if a keyboard
//! is currently connected and the current state of the Caps Lock key on the
//! keyboard that is connected on the bottom status area of the screen.
//! Pressing any keys on the keyboard will cause them to be printed on the
//! screen and to be sent out the UART at 115200 baud with no parity, 8 bits
//! and 1 stop bit. Any keyboard that supports the USB HID BIOS protocol
//! should work with this demo application.
//
//*****************************************************************************
//*****************************************************************************
//
// The ASCII code for a backspace character.
//
//*****************************************************************************
#define ASCII_BACKSPACE 0x08
//*****************************************************************************
//
// The size of the host controller's memory pool in bytes.
//
//*****************************************************************************
#define HCD_MEMORY_SIZE 128
//*****************************************************************************
//
// The memory pool to provide to the Host controller driver.
//
//*****************************************************************************
uint8_t g_pui8HCDPool[HCD_MEMORY_SIZE];
//*****************************************************************************
//
// The size of the keyboard device interface's memory pool in bytes.
//
//*****************************************************************************
#define KEYBOARD_MEMORY_SIZE 128
//*****************************************************************************
//
// The memory pool to provide to the keyboard device.
//
//*****************************************************************************
uint8_t g_pui8Buffer[KEYBOARD_MEMORY_SIZE];
//*****************************************************************************
//
// Declare the USB Events driver interface.
//
//*****************************************************************************
DECLARE_EVENT_DRIVER(g_sUSBEventDriver, 0, 0, USBHCDEvents);
//*****************************************************************************
//
// The global that holds all of the host drivers in use in the application.
// In this case, only the Keyboard class is loaded.
//
//*****************************************************************************
static tUSBHostClassDriver const * const g_ppHostClassDrivers[] =
{
&g_sUSBHIDClassDriver,
&g_sUSBEventDriver
};
//*****************************************************************************
//
// This global holds the number of class drivers in the g_ppHostClassDrivers
// list.
//
//*****************************************************************************
static const uint32_t g_ui32NumHostClassDrivers =
sizeof(g_ppHostClassDrivers) / sizeof(tUSBHostClassDriver *);
//*****************************************************************************
//
// The number of SysTick ticks per second.
//
//*****************************************************************************
#define TICKS_PER_SECOND 100
#define MS_PER_SYSTICK (1000 / TICKS_PER_SECOND)
//*****************************************************************************
//
// Our running system tick counter and a global used to determine the time
// elapsed since last call to GetTickms().
//
//*****************************************************************************
uint32_t g_ui32SysTickCount;
uint32_t g_ui32LastTick;
//*****************************************************************************
//
// The global value used to store the keyboard instance value.
//
//*****************************************************************************
static tUSBHKeyboard *g_psKeyboardInstance;
//*****************************************************************************
//
// This enumerated type is used to hold the states of the keyboard.
//
//*****************************************************************************
enum
{
//
// No device is present.
//
STATE_NO_DEVICE,
//
// Keyboard has been detected and needs to be initialized in the main
// loop.
//
STATE_KEYBOARD_INIT,
//
// Keyboard is connected and waiting for events.
//
STATE_KEYBOARD_CONNECTED,
//
// Keyboard has received a key press that requires updating the keyboard
// in the main loop.
//
STATE_KEYBOARD_UPDATE,
//
// An unsupported device has been attached.
//
STATE_UNKNOWN_DEVICE,
//
// A power fault has occurred.
//
STATE_POWER_FAULT
}
g_eUSBState;
extern const tHIDKeyboardUsageTable g_sUSKeyboardMap;
//*****************************************************************************
//
// The current USB operating mode - Host, Device or unknown.
//
//*****************************************************************************
tUSBMode g_eCurrentUSBMode;
//*****************************************************************************
//
// These defines are used to define the screen constraints to the application.
//
//*****************************************************************************
#define DISPLAY_BANNER_HEIGHT 10
#define DISPLAY_BANNER_BG ClrDarkBlue
#define DISPLAY_TEXT_BORDER 2
#define DISPLAY_TEXT_FG ClrWhite
#define DISPLAY_TEXT_BG ClrBlack
//*****************************************************************************
//
// This variable holds the current status of the modifiers keys.
//
//*****************************************************************************
uint32_t g_ui32Modifiers = 0;
//*****************************************************************************
//
// This is the number of characters that will fit on a line in the text area.
//
//*****************************************************************************
uint32_t g_ui32CharsPerLine;
//*****************************************************************************
//
// This is the number of lines that will fit in the text area.
//
//*****************************************************************************
uint32_t g_ui32LinesPerScreen;
//*****************************************************************************
//
// This is the current line for printing in the text area.
//
//*****************************************************************************
uint32_t g_ui32Line = 0;
//*****************************************************************************
//
// This is the current column for printing in the text area.
//
//*****************************************************************************
uint32_t g_ui32Column = 0;
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// This is the handler for this SysTick interrupt.
//
//*****************************************************************************
void
SysTickIntHandler(void)
{
//
// Update our tick counter.
//
g_ui32SysTickCount++;
}
//*****************************************************************************
//
// This function prints the character out the UART and into the text area of
// the screen.
//
// \param cChar is the character to print out.
//
// This function handles all of the detail of printing a character to both the
// UART and to the text area of the screen on the evaluation board. The text
// area of the screen will be cleared any time the text goes beyond the end
// of the text area.
//
// \return None.
//
//*****************************************************************************
//*****************************************************************************
//
// This function updates the status area of the screen. It uses the current
// state of the application to print the status bar.
//
//*****************************************************************************
void
UpdateStatus(void)
{
//
// Update the status on the screen.
//
if(g_eUSBState == STATE_NO_DEVICE)
{
//
// Keyboard is currently disconnected.
//
UARTprintf("no device\n");
}
else if(g_eUSBState == STATE_UNKNOWN_DEVICE)
{
//
// Unknown device is currently connected.
//
UARTprintf("unknown device\n");
}
else if(g_eUSBState == STATE_POWER_FAULT)
{
//
// Something caused a power fault.
//
UARTprintf("power fault\n");
}
else if((g_eUSBState == STATE_KEYBOARD_CONNECTED) ||
(g_eUSBState == STATE_KEYBOARD_UPDATE))
{
//
// Keyboard is connected.
//
UARTprintf("connected\n");
//
// Update the CAPS Lock status.
//
if(g_ui32Modifiers & HID_KEYB_CAPS_LOCK)
{
UARTprintf("C\n");
}
}
}
//*****************************************************************************
//
// This is the generic callback from host stack.
//
// pvData is actually a pointer to a tEventInfo structure.
//
// This function will be called to inform the application when a USB event has
// occurred that is outside those related to the keyboard device. At this
// point this is used to detect unsupported devices being inserted and removed.
// It is also used to inform the application when a power fault has occurred.
// This function is required when the g_USBGenericEventDriver is included in
// the host controller driver array that is passed in to the
// USBHCDRegisterDrivers() function.
//
//*****************************************************************************
void
USBHCDEvents(void *pvData)
{
tEventInfo *pEventInfo;
//
// Cast this pointer to its actual type.
//
pEventInfo = (tEventInfo *)pvData;
switch(pEventInfo->ui32Event)
{
//
// New keyboard detected.
//
case USB_EVENT_CONNECTED:
{
//
// See if this is a HID Keyboard.
//
if((USBHCDDevClass(pEventInfo->ui32Instance, 0) == USB_CLASS_HID) &&
(USBHCDDevProtocol(pEventInfo->ui32Instance, 0) ==
USB_HID_PROTOCOL_KEYB))
{
//
// Indicate that the keyboard has been detected.
//
UARTprintf("Keyboard Connected\n");
//
// Proceed to the STATE_KEYBOARD_INIT state so that the main
// loop can finish initialized the mouse since
// USBHKeyboardInit() cannot be called from within a callback.
//
g_eUSBState = STATE_KEYBOARD_INIT;
}
break;
}
//
// Unsupported device detected.
//
case USB_EVENT_UNKNOWN_CONNECTED:
{
UARTprintf("Unsupported Device Class (0x%02x) Connected.\n",
pEventInfo->ui32Instance);
//
// An unknown device was detected.
//
g_eUSBState = STATE_UNKNOWN_DEVICE;
UpdateStatus();
break;
}
//
// Device has been unplugged.
//
case USB_EVENT_DISCONNECTED:
{
//
// Indicate that the device has been disconnected.
//
UARTprintf("Device Disconnected\n");
//
// Change the state so that the main loop knows that the device
// is no longer present.
//
g_eUSBState = STATE_NO_DEVICE;
//
// Update the screen.
//
UpdateStatus();
break;
}
//
// Power Fault occurred.
//
case USB_EVENT_POWER_FAULT:
{
UARTprintf("Power Fault\n");
//
// No power means no device is present.
//
g_eUSBState = STATE_POWER_FAULT;
UpdateStatus();
break;
}
default:
{
break;
}
}
}
//*****************************************************************************
//
// USB Mode callback
//
// \param ui32Index is the zero-based index of the USB controller making the
// callback.
// \param eMode indicates the new operating mode.
//
// This function is called by the USB library whenever an OTG mode change
// occurs and, if a connection has been made, informs us of whether we are to
// operate as a host or device.
//
// \return None.
//
//*****************************************************************************
void
ModeCallback(uint32_t ui32Index, tUSBMode eMode)
{
//
// Save the new mode.
//
g_eCurrentUSBMode = eMode;
switch(eMode)
{
case eUSBModeHost:
{
UARTprintf("\nHost Mode.\n");
break;
}
case eUSBModeDevice:
{
UARTprintf("\nDevice Mode.\n");
break;
}
case eUSBModeNone:
{
UARTprintf("\nIdle Mode.\n");
break;
}
default:
{
UARTprintf("ERROR: Bad Mode!\n");
break;
}
}
}
//*****************************************************************************
//
// This is the callback from the USB HID keyboard handler.
//
// \param psKbInstance is ignored by this function.
// \param ui32Event is one of the valid events for a keyboard device.
// \param ui32MsgParam is defined by the event that occurs.
// \param pvMsgData is a pointer to data that is defined by the event that
// occurs.
//
// This function will be called to inform the application when a keyboard has
// been plugged in or removed and any time a key is pressed or released.
//
// \return None.
//
//*****************************************************************************
void
KeyboardCallback(tUSBHKeyboard *psKbInstance, uint32_t ui32Event,
uint32_t ui32MsgParam, void *pvMsgData)
{
char cChar;
switch(ui32Event)
{
//
// New Key press detected.
//
case USBH_EVENT_HID_KB_PRESS:
{
//
// If this was a Caps Lock key then update the Caps Lock state.
//
if(ui32MsgParam == HID_KEYB_USAGE_CAPSLOCK)
{
//
// The main loop needs to update the keyboard's Caps Lock
// state.
//
g_eUSBState = STATE_KEYBOARD_UPDATE;
//
// Toggle the current Caps Lock state.
//
g_ui32Modifiers ^= HID_KEYB_CAPS_LOCK;
//
// Update the screen based on the Caps Lock status.
//
UpdateStatus();
}
else if(ui32MsgParam == HID_KEYB_USAGE_SCROLLOCK)
{
//
// The main loop needs to update the keyboard's Scroll Lock
// state.
//
g_eUSBState = STATE_KEYBOARD_UPDATE;
//
// Toggle the current Scroll Lock state.
//
g_ui32Modifiers ^= HID_KEYB_SCROLL_LOCK;
}
else if(ui32MsgParam == HID_KEYB_USAGE_NUMLOCK)
{
//
// The main loop needs to update the keyboard's Scroll Lock
// state.
//
g_eUSBState = STATE_KEYBOARD_UPDATE;
//
// Toggle the current Num Lock state.
//
g_ui32Modifiers ^= HID_KEYB_NUM_LOCK;
}
else
{
//
// Was this the backspace key?
//
if((uint8_t)ui32MsgParam == HID_KEYB_USAGE_BACKSPACE)
{
//
// Yes - set the ASCII code for a backspace key. This is
// not returned by USBHKeyboardUsageToChar since this only
// returns printable characters.
//
cChar = ASCII_BACKSPACE;
}
else
{
//
// This is not backspace so try to map the usage code to a
// printable ASCII character.
//
cChar = (char)
USBHKeyboardUsageToChar(g_psKeyboardInstance,
&g_sUSKeyboardMap,
(uint8_t)ui32MsgParam);
}
//
// A zero value indicates there was no textual mapping of this
// usage code.
//
if(cChar != 0)
{
UARTprintf((cChar));
}
}
break;
}
case USBH_EVENT_HID_KB_MOD:
{
//
// This application ignores the state of the shift or control
// and other special keys.
//
break;
}
case USBH_EVENT_HID_KB_REL:
{
//
// This applications ignores the release of keys as well.
//
break;
}
}
}
//*****************************************************************************
//
// This function returns the number of ticks since the last time this function
// was called.
//
//*****************************************************************************
uint32_t
GetTickms(void)
{
uint32_t ui32RetVal;
uint32_t ui32Saved;
ui32RetVal = g_ui32SysTickCount;
ui32Saved = ui32RetVal;
if(ui32Saved > g_ui32LastTick)
{
ui32RetVal = ui32Saved - g_ui32LastTick;
}
else
{
ui32RetVal = g_ui32LastTick - ui32Saved;
}
//
// This could miss a few milliseconds but the timings here are on a
// much larger scale.
//
g_ui32LastTick = ui32Saved;
//
// Return the number of milliseconds since the last time this was called.
//
return(ui32RetVal * MS_PER_SYSTICK);
}
//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// This is the main loop that runs the application.
//
//*****************************************************************************
int
main(void)
{
tUSBMode eLastMode;
char *pcString;
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPULazyStackingEnable();
//
// Set the system clock to run at 50MHz from the PLL.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
SYSCTL_XTAL_16MHZ);
//
// Initially wait for device connection.
//
g_eUSBState = STATE_NO_DEVICE;
eLastMode = eUSBModeOTG;
g_eCurrentUSBMode = eUSBModeOTG;
//
// Enable Clocking to the USB controller.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_USB0);
//
// Configure the required pins for USB operation.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_GPIOPinTypeUSBAnalog(GPIO_PORTD_BASE, GPIO_PIN_4 | GPIO_PIN_5);
//ROM_GPIOPinTypeUSBAnalog(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Configure SysTick for a 100Hz interrupt.
//
ROM_SysTickPeriodSet(ROM_SysCtlClockGet() / TICKS_PER_SECOND);
ROM_SysTickEnable();
ROM_SysTickIntEnable();
//
// Enable Interrupts
//
ROM_IntMasterEnable();
//
// Configure UART0 for debug output.
//
ConfigureUART();
//
// Initialize the USB stack mode and pass in a mode callback.
//
USBStackModeSet(0, eUSBModeOTG, ModeCallback);
//
// Register the host class drivers.
//
USBHCDRegisterDrivers(0, g_ppHostClassDrivers, g_ui32NumHostClassDrivers);
//
// Open an instance of the keyboard driver. The keyboard does not need
// to be present at this time, this just save a place for it and allows
// the applications to be notified when a keyboard is present.
//
g_psKeyboardInstance = USBHKeyboardOpen(KeyboardCallback, g_pui8Buffer,
KEYBOARD_MEMORY_SIZE);
//
// Initialize the power configuration. This sets the power enable signal
// to be active high and does not enable the power fault.
//
//USBHCDPowerConfigInit(0, USBHCD_VBUS_AUTO_HIGH | USBHCD_VBUS_FILTER);
//
// Initialize the USB controller for OTG operation with a 2ms polling
// rate.
//
USBOTGModeInit(0, 2000, g_pui8HCDPool, HCD_MEMORY_SIZE);
//
// Open and instance of the keyboard class driver.
//
UARTprintf("Host Keyboard Application\n");
//
// Initial update of the screen.
//
UpdateStatus();
//
// The main loop for the application.
//
while(1)
{
//
// Tell the OTG library code how much time has passed in
// milliseconds since the last call.
//
USBOTGMain(GetTickms());
//
// Has the USB mode changed since last time we checked?
//
if(g_eCurrentUSBMode != eLastMode)
{
//
// Remember the new mode.
//
eLastMode = g_eCurrentUSBMode;
switch(eLastMode)
{
case eUSBModeHost:
pcString = "HOST";
break;
case eUSBModeDevice:
pcString = "DEVICE";
break;
case eUSBModeNone:
pcString = "NONE";
break;
default:
pcString = "UNKNOWN";
break;
}
UARTprintf("USB mode changed to %s\n", pcString);
}
switch(g_eUSBState)
{
//
// This state is entered when they keyboard is first detected.
//
case STATE_KEYBOARD_INIT:
{
//
// Initialized the newly connected keyboard.
//
USBHKeyboardInit(g_psKeyboardInstance);
//
// Proceed to the keyboard connected state.
//
g_eUSBState = STATE_KEYBOARD_CONNECTED;
//
// Update the screen now that the keyboard has been
// initialized.
//
UpdateStatus();
USBHKeyboardModifierSet(g_psKeyboardInstance, g_ui32Modifiers);
break;
}
case STATE_KEYBOARD_UPDATE:
{
//
// If the application detected a change that required an
// update to be sent to the keyboard to change the modifier
// state then call it and return to the connected state.
//
g_eUSBState = STATE_KEYBOARD_CONNECTED;
USBHKeyboardModifierSet(g_psKeyboardInstance, g_ui32Modifiers);
break;
}
case STATE_KEYBOARD_CONNECTED:
{
//
// Nothing is currently done in the main loop when the keyboard
// is connected.
//
break;
}
case STATE_UNKNOWN_DEVICE:
{
//
// Nothing to do as the device is unknown.
//
break;
}
case STATE_NO_DEVICE:
{
//
// Nothing is currently done in the main loop when the keyboard
// is not connected.
//
break;
}
default:
{
break;
}
}
}
}
//*****************************************************************************
//
// Startup code for use with TI's Code Composer Studio.
//
// Copyright (c) 2011-2014 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
//*****************************************************************************
#include <stdint.h>
//*****************************************************************************
//
// Forward declaration of the default fault handlers.
//
//*****************************************************************************
void ResetISR(void);
static void NmiSR(void);
static void FaultISR(void);
static void IntDefaultHandler(void);
//*****************************************************************************
//
// External declaration for the reset handler that is to be called when the
// processor is started
//
//*****************************************************************************
extern void _c_int00(void);
//*****************************************************************************
//
// Linker variable that marks the top of the stack.
//
//*****************************************************************************
extern uint32_t __STACK_TOP;
//*****************************************************************************
//
// External declarations for the interrupt handlers used by the application.
//
//*****************************************************************************
// To be added by user
extern void SysTickIntHandler(void);
extern void USB0OTGModeIntHandler(void);
//*****************************************************************************
//
// The vector table. Note that the proper constructs must be placed on this to
// ensure that it ends up at physical address 0x0000.0000 or at the start of
// the program if located at a start address other than 0.
//
//*****************************************************************************
#pragma DATA_SECTION(g_pfnVectors, ".intvecs")
void (* const g_pfnVectors[])(void) =
{
(void (*)(void))((uint32_t)&__STACK_TOP),
// The initial stack pointer
ResetISR, // The reset handler
NmiSR, // The NMI handler
FaultISR, // The hard fault handler
IntDefaultHandler, // The MPU fault handler
IntDefaultHandler, // The bus fault handler
IntDefaultHandler, // The usage fault handler
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // SVCall handler
IntDefaultHandler, // Debug monitor handler
0, // Reserved
IntDefaultHandler, // The PendSV handler
SysTickIntHandler, // The SysTick handler
IntDefaultHandler, // GPIO Port A
IntDefaultHandler, // GPIO Port B
IntDefaultHandler, // GPIO Port C
IntDefaultHandler, // GPIO Port D
IntDefaultHandler, // GPIO Port E
IntDefaultHandler, // UART0 Rx and Tx
IntDefaultHandler, // UART1 Rx and Tx
IntDefaultHandler, // SSI0 Rx and Tx
IntDefaultHandler, // I2C0 Master and Slave
IntDefaultHandler, // PWM Fault
IntDefaultHandler, // PWM Generator 0
IntDefaultHandler, // PWM Generator 1
IntDefaultHandler, // PWM Generator 2
IntDefaultHandler, // Quadrature Encoder 0
IntDefaultHandler, // ADC Sequence 0
IntDefaultHandler, // ADC Sequence 1
IntDefaultHandler, // ADC Sequence 2
IntDefaultHandler, // ADC Sequence 3
IntDefaultHandler, // Watchdog timer
IntDefaultHandler, // Timer 0 subtimer A
IntDefaultHandler, // Timer 0 subtimer B
IntDefaultHandler, // Timer 1 subtimer A
IntDefaultHandler, // Timer 1 subtimer B
IntDefaultHandler, // Timer 2 subtimer A
IntDefaultHandler, // Timer 2 subtimer B
IntDefaultHandler, // Analog Comparator 0
IntDefaultHandler, // Analog Comparator 1
IntDefaultHandler, // Analog Comparator 2
IntDefaultHandler, // System Control (PLL, OSC, BO)
IntDefaultHandler, // FLASH Control
IntDefaultHandler, // GPIO Port F
IntDefaultHandler, // GPIO Port G
IntDefaultHandler, // GPIO Port H
IntDefaultHandler, // UART2 Rx and Tx
IntDefaultHandler, // SSI1 Rx and Tx
IntDefaultHandler, // Timer 3 subtimer A
IntDefaultHandler, // Timer 3 subtimer B
IntDefaultHandler, // I2C1 Master and Slave
IntDefaultHandler, // Quadrature Encoder 1
IntDefaultHandler, // CAN0
IntDefaultHandler, // CAN1
0, // Reserved
0, // Reserved
IntDefaultHandler, // Hibernate
USB0OTGModeIntHandler, // USB0
IntDefaultHandler, // PWM Generator 3
IntDefaultHandler, // uDMA Software Transfer
IntDefaultHandler, // uDMA Error
IntDefaultHandler, // ADC1 Sequence 0
IntDefaultHandler, // ADC1 Sequence 1
IntDefaultHandler, // ADC1 Sequence 2
IntDefaultHandler, // ADC1 Sequence 3
0, // Reserved
0, // Reserved
IntDefaultHandler, // GPIO Port J
IntDefaultHandler, // GPIO Port K
IntDefaultHandler, // GPIO Port L
IntDefaultHandler, // SSI2 Rx and Tx
IntDefaultHandler, // SSI3 Rx and Tx
IntDefaultHandler, // UART3 Rx and Tx
IntDefaultHandler, // UART4 Rx and Tx
IntDefaultHandler, // UART5 Rx and Tx
IntDefaultHandler, // UART6 Rx and Tx
IntDefaultHandler, // UART7 Rx and Tx
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // I2C2 Master and Slave
IntDefaultHandler, // I2C3 Master and Slave
IntDefaultHandler, // Timer 4 subtimer A
IntDefaultHandler, // Timer 4 subtimer B
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // Timer 5 subtimer A
IntDefaultHandler, // Timer 5 subtimer B
IntDefaultHandler, // Wide Timer 0 subtimer A
IntDefaultHandler, // Wide Timer 0 subtimer B
IntDefaultHandler, // Wide Timer 1 subtimer A
IntDefaultHandler, // Wide Timer 1 subtimer B
IntDefaultHandler, // Wide Timer 2 subtimer A
IntDefaultHandler, // Wide Timer 2 subtimer B
IntDefaultHandler, // Wide Timer 3 subtimer A
IntDefaultHandler, // Wide Timer 3 subtimer B
IntDefaultHandler, // Wide Timer 4 subtimer A
IntDefaultHandler, // Wide Timer 4 subtimer B
IntDefaultHandler, // Wide Timer 5 subtimer A
IntDefaultHandler, // Wide Timer 5 subtimer B
IntDefaultHandler, // FPU
0, // Reserved
0, // Reserved
IntDefaultHandler, // I2C4 Master and Slave
IntDefaultHandler, // I2C5 Master and Slave
IntDefaultHandler, // GPIO Port M
IntDefaultHandler, // GPIO Port N
IntDefaultHandler, // Quadrature Encoder 2
0, // Reserved
0, // Reserved
IntDefaultHandler, // GPIO Port P (Summary or P0)
IntDefaultHandler, // GPIO Port P1
IntDefaultHandler, // GPIO Port P2
IntDefaultHandler, // GPIO Port P3
IntDefaultHandler, // GPIO Port P4
IntDefaultHandler, // GPIO Port P5
IntDefaultHandler, // GPIO Port P6
IntDefaultHandler, // GPIO Port P7
IntDefaultHandler, // GPIO Port Q (Summary or Q0)
IntDefaultHandler, // GPIO Port Q1
IntDefaultHandler, // GPIO Port Q2
IntDefaultHandler, // GPIO Port Q3
IntDefaultHandler, // GPIO Port Q4
IntDefaultHandler, // GPIO Port Q5
IntDefaultHandler, // GPIO Port Q6
IntDefaultHandler, // GPIO Port Q7
IntDefaultHandler, // GPIO Port R
IntDefaultHandler, // GPIO Port S
IntDefaultHandler, // PWM 1 Generator 0
IntDefaultHandler, // PWM 1 Generator 1
IntDefaultHandler, // PWM 1 Generator 2
IntDefaultHandler, // PWM 1 Generator 3
IntDefaultHandler // PWM 1 Fault
};
//*****************************************************************************
//
// This is the code that gets called when the processor first starts execution
// following a reset event. Only the absolutely necessary set is performed,
// after which the application supplied entry() routine is called. Any fancy
// actions (such as making decisions based on the reset cause register, and
// resetting the bits in that register) are left solely in the hands of the
// application.
//
//*****************************************************************************
void
ResetISR(void)
{
//
// Jump to the CCS C initialization routine. This will enable the
// floating-point unit as well, so that does not need to be done here.
//
__asm(" .global _c_int00\n"
" b.w _c_int00");
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives a NMI. This
// simply enters an infinite loop, preserving the system state for examination
// by a debugger.
//
//*****************************************************************************
static void
NmiSR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives a fault
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
FaultISR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}
//*****************************************************************************
//
// This is the code that gets called when the processor receives an unexpected
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
IntDefaultHandler(void)
{
//
// Go into an infinite loop.
//
while(1)
{
}
}