Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hi Forum,
through my last posts I manage to build a stable version of my program and as a result it works flawless on my own hardware.
As a next step I want to use a serial UART bootloader to flash my controller via the UART0 interface. Trying to achieve this I faced some obstacles which left me behind a little bit confused. Besides my program I want to use, I cannot debug the bootloader when flashed, because it always stops when copying the code image from flash to SRAM. I also tried that with my EK-TM4C1294 but could not succeed there either.
Starting here at the start of the program in my startup script:
_c_int00: .asmfunc b ResetISR
the program manages to come to the
;; Initialize the processor.
;;
bl ProcessorInit
routine with the error mentioned below.
I could imagine that this is just a settings things, however my assembler lessons are long ago and I cannot image why I can not step through this.
Regards,
Volker