Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN
Hi,
I am using TMS570LS1224 Launch pad to interface a booster pack. The requirement is to use eQEP_2 module to interface with Quadrature Encoder.
GIOA_5, GIOA_2, GIOA_1 at J4 on Launchpad are used to get Quadrature Encoder inputs (A,B and I) from Encoder at 5V to these GIO pins at 3.3V after a level shifter.
GIOA pins are configured as inputs and pull ups.
My issue is when I connect Encoder, through level shifter, I get correct Encoder Signals(A,B and I) on GIOA_5, GIO_2 and GIO_1 respectively. But at the same time I see Encoder (B pulse train ) on EQEP2I pin at J11(pin 12) without any connections.
I am unable to use eQEP module since I am not getting the encoder Index pulse on this pin,
GIOA_2 and eQEP2I are pinmuxed.
Is this creating a problem?
Regards,
Poorva