Part Number: TM4C123BH6PZ
Question:
I see this processor can run with its own internal oscillator.. does that run at the max speed of the part.. or??
From what I can tell from the datasheet - the maximum self-clocking speed is 16MHz (please confirm).
And the maximum external crystal speed is 25MHz...
So it I think it means, no, it can't run at its full speed capability with self clocking.
Thanks!