Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: CC1310
Hi All,
Please tell me about Tiva-C's UART Flow Control with TI-RTOS.
Customer communicating with UART between Tiva-C and CC1310, and it was connected both CTX and RTS, but it can not communicate.
When checking the communication waveform with the oscilloscope, both signals were pull-down and were always asserted.
Therefore, when RTS Pin of CC1310 was Pull-UP with PIN_Config(), communication of Tiva-C(Tx) -> CC1310(Rx) could be controlled.
They tried Pull-UP of Tiva-C's RTS pin in the same way, but I could not set it with Pin_Config().
They tried to Pull-UP with external resistance, but if they make it BIOS_Start with TI-RTOS the RTS pin will be asserted.
(Up to BIOS_Start, RTS was Pull-Up.)
So please tell me about the following contents.
1. Can Tiva-C use UART function and built-in Pull-UP function at the same time?
2. Can I control Tiva-C's UART Flow Control with TI-RTOS?
Best Regards,
Takashi