Part Number: LAUNCHXL2-TMS57012
Other Parts Discussed in Thread: HALCOGEN
Tool/software: TI C/C++ Compiler
currently i'm using halcogen as a driver to MCU components .... in it's api there are several functions which will be called upon an interrupt event (assuming VIM module appropriate settings ) .... i'm wondering which part of the codes which generated by the halcogen cause that for example sciNotification() function to be called when SCI/LIN module receive a character.
i'm skim include header files but find nothing ...
if the question is unclear just tell me to provide more information .... thanks in advance .