Part Number: SW-EK-TM4C1294XL
Hello
I am working with the boot loader example project and have it working with the serial UART correctly. When I change the project to use CAN in the bl_config.h and recompile the project I get the errors
Description Resource Path Location Type
#20 identifier "CAN_RX_PIN_PCTL" is undefined bl_can.c /boot_serial/boot_loader line 1398 C/C++ Problem
Description Resource Path Location Type
#20 identifier "CAN_TX_PIN_PCTL" is undefined bl_can.c /boot_serial/boot_loader line 1398 C/C++ Problem
I cant find these defines anywhere.
Thanks
-Chris