This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/EK-TM4C1294XL: Is there socket for networking available in TM4C1294XL

Part Number: EK-TM4C1294XL


Tool/software: TI-RTOS

1)

Is there socket library available for TM4C1294XL Evaluation Kit because card has an Ethernet connector.  I mean that is the socket available for programmers as winsock2.h is in Windows and as sys/socket.h is in Linux based operating systems?  I have seen that in TM4C1294XL has http-level connection libraries but is there available TCP/UDP level sockets in TM4C1294XL?

2)

Is TI-RTOS available for TM4C1294XL when using free version of Code Composer Studio 7.2?