Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129DNCPDT: Find MCU with 2xUSB interface (USB2.0 PHY embedded MCU)

Part Number: TM4C129DNCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL

We are using TM4C129DNCPDT for production and integrate SPI to USB HOST chip,

 for new generation products, we want to find MCU have 2 usb ports without HW interface translation( no SPI, no ULPI) 

1 port as device (link PC for DAQ, control device)

1 port as Host (connect DUT, control DUT)

Does Ti have embedded HS USB2.0 PHYsolution?

  • Hi Chih,

    The TM4C1294NCDT USB peripheral Tivaware software library functions only support device or host mode respectively to a single endpoint. The USB PHY directly supports an external HUB chip for a custom PCB up to 480MBPS data transfer rates. That gives custom PCB multiple USB ports for several connected HID devices, e.g. mouse/keyboard etc.. Not sure if the DK-TM4C1294X version host hub library functions support an external USB hub chip directly though it seems plausible.

    Perhaps install the USB library and Host hub example found under DK-TM4C1294X product to aid in your discovery process. As to JTAG support via USB virtual device mode; TI has never released to public domain the embedded code written for TM4C123G ICDI Stellaris USB virtual emulator shipped on the EK-TM4C1294XL launch pad. Engineers thusly employ JTAG header on a custom PCB for debug DUT control purpose.

  • Moderator please mark this question Answered for reasons given.