I checked the documentation SPNZ233A(Errata for Silion B) and SPNA233A(Herculas PLL Advisory SSWF021#45 ).
They say once the PLL is locked properly, it can be disabled or enabled without any issue.
My question is:
- In case that configuring and locking PLL are properly done, if I disable PLL again and change the values of PLLCTL1/2/3, and then enable the PLL, do I need the workround for SSWF021#45 at this time?
- In this topic: https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/554006/2025900, it says the workaround for SSWF021#45 is not 100% guaranteed effective. Is this still true for RM57L843?