This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: Setup two EKs

Part Number: EK-TM4C1294XL

2843.EKSetup.htm

I'm trying to set up uart communication (U5) between two EK-TM4C1294XL. The EK on the bottom is the

transmitter EK, the one on top is the receiver EK.

Both uarts are setup in 9 bit mode with fifo disabled. The 9bit output is displayed through U0 on PuTTY

formatted as a 16 bit integer.

Every 10 seconds, the transmitter EK sends a hex number to the receiver EK. When debugged alone (no

receiver EK),  the transmit byte is displayed on PuTTY correctly. The receiver EK should send back a different

byte in response. Both uarts are set up with an interrupt on receive mode only.

Should one EK have an external power source? I currently have both EKs powered through the same computer.

The receiver EK is not responding correctly. I have not seen the uart outputs on the scope yet, I will if I must.

The EKs are listed on separate com ports, but I see PuTTY working only on the transmitter EK com port. It doesn't

matter which EK is hooked up to the U0 Rx jumper, the only byte I see on PuTTY is the transmitted byte.

Is it possible for an USB stick to independently power an EK? Will the USB stick example help set this up?

Or should I look for a battery for this?

Thank you,

Priya

 

  • To more quickly/easily (i.e. KISS) test such a hook-up - would it not be easier to "Start" with the more "normal/customary" 8 bit UART config?

    Starting this way - you could then "test/verify" that indeed - both boards provide a functional, UART Output.

    Note - it is vital that you have created a "common ground" between each EK.     Have you insured that - have you "ohmed that out" (w/power removed?)

    I'm concerned about the use of your "U0 RX jumper" - which I fear - may prevent the delivery of UART to UART communication - due to its "one device at a time" methodology.     Does this "one at a time, limited mechanical connection" not insure that - when in the RX position - the TX signal cannot be received by the RX?       How then does the RX UART then "know" that it has been directed/commanded to transmit?     To avoid this, "Failed Command Reception" you may write a simple program which causes the RX UART to output a char. every second - independent of data arrival.     Your first goal - I believe - is to achieve output from the board designated as, "UART RX."

    I suppose that the RX jumper may (only) route to the PC - charged w/monitoring UART output - which will (not) disrupt the communication link - yet your description does not make this fact sufficiently clear.

    I would turn my attention to achieving the simplest output from the RX UART (that being 8 bit) and only proceed once that hurdle has been cleared...

    Power must always be proper - if in any doubt - "Convenient Power" (introduced from the PC via board's USB receptacle) should NEVER trump "Proper Power."    Have you measured the voltage - both (assumed) 5V (via USB) and 3V3 (to the MCU) upon each board - when operating?      You speak also of, "using a USB stick to independently power."     To clarify - are you speaking of a non-PC power supply - which connects to the EK - via a USB receptacle?     I don't know your boards -  "you" must insure that the (expected), powering 5V proves adequate for (both) EKs - during every aspect of operation - that's just BASIC!

  • Maybe someone from TI can respond to this? I have U0 set up for display on both EKs. I'm not using U0 currently, I am observing U5 outputs on the scope now. I am unable to debug the receiver EK is both EKs are connected to the same computer, it seems like CCS programs both EKs with the same project output. Which is why an external power source will make things easier.

    As far as the scope output, I can see the transmitted byte from EK1(U5Tx) received on EK2 (U5Rx). This is in uart 9 bit mode. But there is no response from Ek2 U5 Tx. I have both U5 to receive on interrupt. Soon after EK2 receives a byte, I am transmitting the response byte in the uart interrupt handler function.
  • I too hope that the vendor can & will respond.

    Perhaps in the future - you may note the requirement for, "Only Vendor Response!" - which would have "saved" my time/effort in your behalf!    It is notable that ALL of my points were dismissed (minus any thanks)  - it is expected that vendor will ask for (similar) clarification...     Your post "begs" for a clear diagram - which may add (some) "very required" clarity...

  • Thank you for your time. It is possible the vendor's response is easier to understand.
  • Continuing with cb1's questions

    Are you using the same supply (as well as checking the levels) for both boards? Note, I don't think you are assured the power supplies are the same if you use two different USB ports from your PC. Definitely not if using two powered hubs.

    If not have you connected the commons? You probably should in any case, maybe through a resistor. If the two boards are in different power domains all bets are off.

    Also another vote for testing with standard 8 bit mode.

    Robert
  • Note that you "just now" added file EKSetup.htm. The vendor's response - along w/"another" - are both hoped to be, "easier to understand." Indeed - verifying a "Common Ground" connection - between each EK board - (may) overchallenge!
  • cb1_mobile-- I don't understand your responses.....

    Maybe you just saw EKSetup.htm? It has always been the first part of my original post.
  • Hello Priya,

    Have you been able to verify that the 8-bit mode UART works as expected for starters? This would confirm if your hardware is setup correctly which seems to be the focus on your current concerns.

    I have no experience with 9-bit UART mode, so let's start with 8-bit mode and make sure all hardware works as intended. Then the issue becomes a matter of software adjustment to account for the changes with 9-bit mode. Also using 8-bit mode will allow for better use of UART terminal software to validate the hardware setup is correct. The uart_echo example should be a good place to start with this.

    I am also unsure of the connections you have made when it concerns the jumpers vs wires. Can you provide full detail on all the connections made? The image isn't very useful for me to see all details.

    Also have you tied the GND potential on each EK board together? It would be a prudent step to make sure both boards are operating from the same GND level.

    Priya Nadathur70 said:
    Should one EK have an external power source? I currently have both EKs powered through the same computer.

    I don't think this should be necessary, modern PC's should provide ample power on both ports. If you want to verify, the portion of cb1's post concerning power and measuring voltages is quite applicable though.

    Also just as an FYI, we have a quite old app note on 9-bit mode from the old Stellaris devices, you might find some useful in here if you haven't yet found this: http://www.ti.com/lit/an/spma032/spma032.pdf

  • Thank you for your responses and repetitions. The handshaking between the two EKs works fine in 8 bit mode. Both USB ports supply 5V. I am reading through the app note about 9 bit uarts and will be back later if I have more questions.

    Priya
  • Let the record show that (newly) introduced "handshaking" (reportedly) works fine - yet there is NO clear confirmation of (normal) UART Data-Transfer Success!     (i.e. Krazy-Making)

    KISS - like "LIKE" (both banned here) directs you to employ simple "8 Bit UART Mode" - insure that works well - prior to entering the "9 Bit Swamp."     (which some (promise) to drain...)

  • cb1-- what are you commenting on/asking about? I looked at U5 Tx from EK1 on the scope and U5 Tx from EK2 on the scope as well. LEDs are blinking on both EKs when the transfer happens. I didn't take a screenshot though.
  • My friend - you (suddenly - and w/out explanation) used the word "handshaking" - always & only (earlier) you wrote,

    "I have not seen the uart outputs"
    and
    "the only byte I see on PuTTY is the transmitted byte."

    Thus - should we not question your NEW use of  "handshaking" which was unexplained?       (and most usually - denotes a single bit which toggles to confirm operation.)

    Did you mean - instead - to write that you NOW are able to "see" the RX UART's transmitted byte?     Or - is it just the "LEDs" which are responding - and STILL no UART_RX transfer?      That's not at all clear - and has caused my (proper) comment. 

  • I used 8 bit mode. I transmitted 0x50 and acknowledged with 0x05. So it was easy to see on the scope the response was happening through the EK2 uart. I did not look at PuTTY. I don't know yet why 9 bit mode did not do the same thing.
  • Priya Nadathur70 said:
    I used 8 bit mode.

    Good that - follows "KISS" - surely your best path to success.    (and was suggested by myself & others)

    Priya Nadathur70 said:
    I transmitted 0x50 and acknowledged with 0x05.

    Now this is good news - yet you described this (first time, byte transmit SUCCESS) as "handshaking!"     (technically it is - but was too vague to be useful and "broke from your past UART BYTE" descripitions.)

    It is hard enough to "diagnose tech issues remotely" - introducing brand new terms (i.e. handshaking) - minus (any) explanation - is NOT in your best interest...

    The fact that "8 Bit Mode is working" (as was suspected) now provides (some) confidence in your interconnects & (programming of both MCUs) - and should "set the stage" for your "9 bit exercise."

    As I see it - you are best advised to (for now) abandon any thought of UART_RX "responding" to UART_TX" - instead simply have UART_RX (continually) output chars. @ 1Hz (first in 8 bit mode to confirm the code change) and once that's been confirmed - only then "Switch to 9 Bit Mode" - and determine if PuTTY recognizes such data...     This is a perfect illustration of "KISS" (one step at a time) which best speeds & insures your project's success!

  • cb1_mobile said:
    - only then "Switch to 9 Bit Mode" - and determine if PuTTY recognizes such data...    

    Does Putty deal well with 9 bit data? We've had indication in the past here that it does not and most terminal emulators don't.


    Robert

  • As a work around to PuTTY not dealing with 9 bit data, I am printing a 16 bit integer through U0.
    I have to look more closely at the 9 bit transmit on the scope.
  • It is STILL URGED - independent of PuTTY's performance - that you NOT, "Hold the 9 Bit Mode HOSTAGE" to a, "Command-Response" type of operation.

    As earlier advised - enabling the UART_RX device to simply, "Continually Output - at ~1Hz" (via a change to your existing "UART_RX" program) eliminates any such "hostage holding!"     As always - such complies w/"KISS" - which proves always helpful and speeds/eases your path to success...   (even though - and especially though - this powerful "KISS" technique is never mentioned - nor promoted - here!)    And users - left to their "unguided, overly broad instincts" continue to flounder...

  • cb1 -- In plain English what are you saying?
  • For now - have your "UART_RX" continually output "9 Bits" - with NO DEPENDENCE upon RECEIVING DATA from your UART_TX!     Note that you "MUST CHANGE YOUR CODE SO THAT UART_RX CONTINUALLY OUTPUTS A CHAR - WITH NO OTHER CONDITIONS!    (I do not know how to make that more clear!)

    This "frees" UART_RX from unwanted complexity - at this early stage. You simply seek to output "9 Bit UART" - which can be viewed on a scope (for sure) and iirc - (sometimes) upon a serial terminal. (we've done such - I cannot recall which terminal, though)

    It is HARD to know how you fail to characterize the earlier writing, (in bold) "Continually Output - at ~1Hz" as "beyond plain English."

  • Remember that not all bytes are received in 9-bit mode

    '123 Manual said:

    13.3.7 9-Bit UART Mode

    The UART provides a 9-bit mode that is enabled with the 9BITEN bit in the UART9BITADDR register. This feature is useful in a multi-drop configuration of the UART where a single master connected to multiple slaves can communicate with a particular slave through its address or set of addresses along with a qualifier for an address byte. All the slaves check for the address qualifier in the place of the parity bit and, if set, then compare the byte received with the preprogrammed address. If the address matches, then it receives or sends further data. If the address does not match, it drops the address byte and any subsequent data bytes. If the UART is in 9-bit mode, then the receiver operates with no parity mode. The address can be predefined to match with the received byte and it can be configured with the UART9BITADDR register. The matching can be extended to a set of addresses using the address mask in the UART9BITAMASK register. By default, the UART9BITAMASK is 0xFF, meaning that only the specified address is matched.

    When not finding a match, the rest of the data bytes with the 9th bit cleared are dropped. If a match is found, then an interrupt is generated to the NVIC for further action. The subsequent data bytes with the cleared 9th bit are stored in the FIFO. Software can mask this interrupt in case μDMA and/or FIFO operations are enabled for this instance and processor intervention is not required. All the send transactions with 9-bit mode are data bytes and the 9th bit is cleared. Software can override the 9th bit to be set (to indicate address) by overriding the parity settings to sticky parity with odd parity enabled for a particular byte. To match the transmission time with correct parity settings, the address byte can be transmitted as a single then a burst transfer. The Transmit FIFO does not hold the address/data bit, hence software should take care of enabling the address bit appropriately.

     

    Robert

  • Thank you for your replies and pointers. In 9 bit mode, the transmitter EK1 is showing a 9 bit output on the scope. I made sure I was transmitting a byte that would need 9 bits x143. The peripheral EK2's address is 0xA1. I have the 9 bit mode set up this way in the receiver EK2:

    UART9BitAddrSet(UART5_BASE, 0xA1, 0xFF);
    // UART9BitAddrSet(UART5_BASE, 0x0, 0xFF);
    UART9BitEnable(UART5_BASE);
    UARTFIFODisable(UART5_BASE);

    The transmitter EK1 is set up for 9 bit uart as follows:
    UART9BitAddrSet(UART5_BASE, 0xA1, 0xFF);
    UART9BitEnable(UART5_BASE);
    UARTFIFODisable(UART5_BASE);
    UART9BitAddrSend(UART5_BASE, 0xA1);

    While I can see the U5Rx receive this 9 bit value on the scope, the LED on EK2 does not blink on receiving this byte. I also have a 1 second periodic timer on EK2 independently transmitting byte 0x10b. No activity at all on U5Tx, just a high voltage level on the scope. Is something not right in the address setup between the 2 EKs?

    Regards,
    Priya
  • Priya Nadathur70 said:
    I also have a 1 second periodic timer on EK2 independently transmitting byte 0x10b. No activity at all on U5Tx, just a high voltage level on the scope.

    This appears to be your acceptance of my suggestion - "Generate 9 Bit UART Output - WITHOUT ANY DEPENDENCY AT ALL - ESPECIALLY "DATA RECEIPT!"     Is this the case?

    Note that "0x10b" does NOT require 9 bits - might this compromise 9 Bit output?   (doubtful - but can be quickly tested/resolved.)

    I would quickly switch to 8 Bit UART Output - and see if the scope (then) reveals "normal" UART Output.    If so - do report...

  • Priya Nadathur70 said:
    I also have a 1 second periodic timer on EK2 independently transmitting byte 0x10b. No activity at all on U5Tx, just a high voltage level on the scope.

    Why would you expect any? That does not match the address you set.

    You do realize that the ninth bit is only used for addresses don't you?

    Robert

  • cb1_mobile said:
    Note that "0x10b" does NOT require 9 bits

    that's 100001011 in binary. I count nine bits. In fact, I rather suspect having the ninth bit set is at least part of the issue.

    Robert

  • In MDB, I understand when master transmits to peripheral, the ninth bit indicates its an address byte. Dropping the 9th bit in 0x143, I thought 0xa1 will be the address. Is it something else?

    For EK2, the timer is independent of uart receive. I will check things out in 8 bit mode.

    Thank you,
    Priya
  • Priya Nadathur70 said:
    In MDB, I understand when master transmits to peripheral, the ninth bit indicates its an address byte.

    Yes, that's typical for a nine bit protocol.

    Priya Nadathur70 said:
    Dropping the 9th bit in 0x143, I thought 0xa1 will be the address

    Um, if you drop the ninth bit in 0x143 you get 0x43. But the concept of dropping the ninth bit makes little sense. You add the address bit to the output via a particular TIVAWare function IIRC.

    However, that's also not what you claimed. You clamed you were sending 0x10B. So what are you actually sending? And at this point probably at least as important, how are you sending?

    Robert

  • MDB says LSB indicates address bit. I dropped bit 0 to get A1 as the peripheral address.

    0x10B was a randomly chosen byte that will look different from 143 on the scope coming from ek2. I am sending this from the timer interrupt handler function using UartCharPut.

    Thanks,
    Priya
  • Priya Nadathur70 said:
    I am sending this from the timer interrupt handler function using UartCharPut.

    How? We need to see an example of your code. UartCharPut won't be able to send 9 bit 'characters' since the UART doesn't support that (almost no UART does).

    Priya Nadathur70 said:
    MDB says LSB indicates address bit. I dropped bit 0 to get A1 as the peripheral address.

    That's wrong in almost every respect on the hardware.

    The ninth bit is the parity bit.

    The UART send the bits in order from LSB to MSB followed by the parity bit.

    If MDB reverses these bits, which seems a very odd thing to do, then you will not be able to use the TM4Cs nine bit HW support but will need to created your own in SW. My suspicion is you've mis-interpreted something*.

    Robert

    * In fact a quick peruse of the standard also indicates you've read it wrong. The address bit (mode bit) is not the lsb. See section 2.1 of version 4

    LSB       --->                        MSB

    Start 0 1 2 3 4 5 6 7 Mode Stop

  • Yes, I realized the MDB doc shows the LSB on the left. Does this mean I can't use the TIVA 9 bit uart APIs for MDB? Only the Stellaris seems to have APIs for software 9 bit uart. The LED inside the timer interrupt handle in EK2 is blinking every second. So, its definitely a address problem with the uart in 9bit mode that makes the EK2 not transmit a response. It seems complicated to write a 9 bit software uart, isn't it?

    Thanks,
    Priya
  • Priya Nadathur70 said:
    Yes, I realized the MDB doc shows the LSB on the left.

    Did you also note that the mode bit was in the MSB position?

    Priya Nadathur70 said:
    Does this mean I can't use the TIVA 9 bit uart APIs for MDB?

    No, it means you've confused yourself.

    Priya Nadathur70 said:
    Only the Stellaris seems to have APIs for software 9 bit uart.

    It would be shocking if they didn't work in the same fashion.

    Priya Nadathur70 said:
    It seems complicated to write a 9 bit software uart, isn't it?

    You do need to have a clearer picture of what is happening than you appear to have currently.

    First stop thinking of 9 bit mode as using a 9 bit value. It doesn't. It uses an 8 bit value plus an additional flag bit. The setting of this bit determines if the 8 bit value is a data bit or an address bit. This bit is managed separately from the data and the TIVA APIs reflect that with a separate call to send an eight bit data byte with the flag bit set.

    Robert

  • Robert,

    To clarify with a numeric example:

    This is byte 0x43. From EK1, I am transmitting x43. I see this on the scope. In 9 bit mode

    the duration on the scope would be 11 bits long. The address sent from UART9BitAddrSet

    and UART9BitAddrSend APIs are both 0x43. From EK2, I want to transmit 0x21 to see the response

    clearly on the scope. I am still not seeing anything sent from EK2, though x43 is being received by EK2.

    What am I missing?

    Thanks,

    Priya

    uart
    Start bit LSB MSB Mode Stop
    0 1100 0010 1

    1

  • Priya Nadathur70 said:

    From EK2, I want to transmit 0x21 to see the response

    clearly on the scope. I am still not seeing anything sent from EK2

    What are you doing to do this? You still haven't presented your code for this.

    Robert

  • Here is the code for EK2. This EK receives x43 from EK1 and sends back x21.
    Thanks,
    Priya

    uint32_t g_ui32SysClock;

    unsigned char txcomplete = 0;
    unsigned char timerComplete = 0;
    uint8_t TrxBuffer[1] = {0x21};
    uint8_t i = 0;
    void UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count);
    void Timer3IntHandler(void);

    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif

    //*****************************************************************************
    //
    // Send a string to the UART.
    //
    //*****************************************************************************
    void
    UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
    {
    //
    // Loop while there are more characters to send.
    //

    while(ui32Count--)
    {
    //
    // Write the next character to the UART.

    UARTCharPut(UART5_BASE, *pui8Buffer++);
    // UARTprintf("%x ", TrxBuffer[i++]);
    #if 0
    // Blink the LED to show a character transfer is occuring.
    //
    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

    //
    // Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
    //
    SysCtlDelay(g_ui32SysClock / (1000 * 3));

    //
    // Turn off the LED
    //
    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
    #endif
    }
    }

    void Timer3IntHandler(void)
    {
    // Clear the timer interrupt
    TimerIntClear(TIMER3_BASE, TIMER_TIMA_TIMEOUT);

    // Blink the LED to show a character transfer is occuring.
    //
    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

    //
    // Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
    //
    SysCtlDelay(g_ui32SysClock / (1000 * 3));

    //
    // Turn off the LED
    //
    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);

    UARTSend(TrxBuffer, 1);
    i = 0;

    timerComplete = 1;

    }

    //*****************************************************************************
    //
    // The UART interrupt handler.
    //
    //*****************************************************************************
    void
    UARTIntHandler(void)
    {
    uint32_t ui32Status;

    //
    // Get the interrrupt status.
    //
    ui32Status = UARTIntStatus(UART5_BASE, true);

    //

    //
    // Clear the asserted interrupts.
    //
    UARTIntClear(UART5_BASE, ui32Status);

    // Receive uart char
    while(ROM_UARTCharsAvail(UART5_BASE))
    {
    //
    // Read the next character from the UART and write it back to the UART.
    //

    UARTCharGet(UART5_BASE);

    }

    // Blink the LED to show a character transfer is occuring.
    //
    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

    //
    // Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
    //
    SysCtlDelay(g_ui32SysClock / (1000 * 3));

    //
    // Turn off the LED
    //
    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
    }



    //*****************************************************************************
    //
    // This example demonstrates how to send a string of data to the UART.
    //
    //*****************************************************************************
    int
    main(void)
    {
    uint32_t ui32Period;

    //
    // Set the clocking to run directly from the crystal at 120MHz.
    //
    g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
    SYSCTL_OSC_MAIN |
    SYSCTL_USE_PLL |
    SYSCTL_CFG_VCO_480), 120000000);
    //
    // Enable the GPIO port that is used for the on-board LED.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
    //
    // Enable the GPIO pins for the LED (PN0).
    //
    ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0|GPIO_PIN_1);


    //
    // Enable the peripherals used by this example.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);

    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

    //
    // Enable processor interrupts.
    //
    ROM_IntMasterEnable();

    SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER3);
    TimerConfigure(TIMER3_BASE, TIMER_CFG_PERIODIC);

    ui32Period = g_ui32SysClock/2;
    TimerLoadSet(TIMER3_BASE, TIMER_A, ui32Period-1);

    IntEnable(INT_TIMER3A);
    TimerIntEnable(TIMER3_BASE, TIMER_TIMA_TIMEOUT);
    IntMasterEnable();

    TimerEnable(TIMER3_BASE, TIMER_A);

    //
    // Set GPIO A0 and A1 as UART pins.
    //
    GPIOPinConfigure(GPIO_PC6_U5RX);
    GPIOPinConfigure(GPIO_PC7_U5TX);
    ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);


    //
    // Configure the UART for 9600, 8-N-1 operation.
    //
    ROM_UARTConfigSetExpClk(UART5_BASE, g_ui32SysClock, 9600,
    (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
    UART_CONFIG_PAR_NONE));


    GPIOPinConfigure(GPIO_PA0_U0RX);
    GPIOPinConfigure(GPIO_PA1_U0TX);
    ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

    UARTStdioConfig(0, 9600, g_ui32SysClock);


    UART9BitAddrSet(UART5_BASE, 0x43, 0xFF);
    UART9BitEnable(UART5_BASE);


    UARTFIFODisable(UART5_BASE);

    //
    // Enable the UART interrupt.
    //
    ROM_IntEnable(INT_UART5);
    ROM_UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT | UART_INT_9BIT);
    // ROM_UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT);
    // ROM_UARTIntEnable(UART5_BASE, UART_INT_TX | UART_TXINT_MODE_EOT | UART_INT_9BIT);
    // ROM_UARTIntEnable(UART5_BASE,UART_INT_TX|UART_TXINT_MODE_EOT | UART_INT_9BIT | UART_INT_RX|UART_INT_RT);



    while(1);
    }
  • Use the past code </> option. The result is far more readable.

    Let's start with the interrupt routine

    void
     UARTIntHandler(void)
     {
     uint32_t ui32Status;
    
     //
     // Get the interrrupt status.
     //
     ui32Status = UARTIntStatus(UART5_BASE, true);
    
     //
    
     //
     // Clear the asserted interrupts.
     //
     UARTIntClear(UART5_BASE, ui32Status);
    
     // Receive uart char
     while(ROM_UARTCharsAvail(UART5_BASE))
     {
     //
     // Read the next character from the UART and write it back to the UART.
     //
    
     UARTCharGet(UART5_BASE);
    
     }
     // Blink the LED to show a character transfer is occuring.
     //
     GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);
    
     //
     // Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
     //
     SysCtlDelay(g_ui32SysClock / (1000 * 3));
    
     //
     // Turn off the LED
     //
     GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
     }

    Breaking out pieces for comment.

    This

     // Get the interrrupt status.
     //
     ui32Status = UARTIntStatus(UART5_BASE, true);
    
     //
    
     //
     // Clear the asserted interrupts.
     //
     UARTIntClear(UART5_BASE, ui32Status);
    

    is good provided you properly deal with the status result later. The problem is you don't

     // Receive uart char
     while(ROM_UARTCharsAvail(UART5_BASE))
     {
     //
     // Read the next character from the UART and write it back to the UART.
     //
    
     UARTCharGet(UART5_BASE);
    
     }

    And here's the problem, you never deal with the other interrupts. Specifically you never deal with the 9-bit match receive interrupt. This, despite the fact that you enabled it.

    And this:

     //
     // Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
     //
     SysCtlDelay(g_ui32SysClock / (1000 * 3));

    is a big no-no

    Robert

  • I changed the LED blinking code to toggle without any delays. This made both EKs transmit correctly on timer interrupts. However receive uart in 9 bit mode is not working with either EK.

    Here is the updated code for EK2.

    I appreciate the code review and feedback.

    Thanks,

    Priya

    uint32_t g_ui32SysClock;

    unsigned char txcomplete = 0;
    unsigned char timerComplete = 0;
    uint8_t TrxBuffer[1] = {0x21};
    uint8_t i = 0;
    void UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count);
    void Timer3IntHandler(void);


    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif

    //*****************************************************************************
    //
    // Send a string to the UART.
    //
    //*****************************************************************************
    void
    UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
    {
        //
        // Loop while there are more characters to send.
        //

        while(ui32Count--)
        {
            //
            // Write the next character to the UART.

            UARTCharPut(UART5_BASE, *pui8Buffer++);
    //        UARTprintf("%x ", TrxBuffer[i++]);

        }
    }

    void Timer3IntHandler(void)
    {
        // Clear the timer interrupt
        TimerIntClear(TIMER3_BASE, TIMER_TIMA_TIMEOUT);

        // Blink the LED to show a character transfer is occuring.

        if(GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1))
                {
                    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
                }
        else
                {
                    GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 2);
                }

        UARTSend(TrxBuffer, 1);
        i = 0;

        timerComplete = 1;

    }

    //*****************************************************************************
    //
    // The UART interrupt handler.
    //
    //*****************************************************************************
    void
    UARTIntHandler(void)
    {
        uint32_t ui32Status;

        //
        // Get the interrrupt status.
        //
        ui32Status = UARTIntStatus(UART5_BASE, true);
        uint8_t interrupt_type = (uint8_t) ((ui32Status & 0x1000) >> 12);

        //

        //
        // Clear the asserted interrupts.
        //
        UARTIntClear(UART5_BASE, ui32Status);

        if (interrupt_type == 1){
            // Receive uart char
                 while(UARTCharsAvail(UART5_BASE))
                 {
                     //
                     // Read the next character from the UART and write it back to the UART.
                     //

                     UARTCharGet(UART5_BASE);
                 }

        if(GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1))
            {
                GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
            }
        else
            {
                GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 2);
            }
        }

    }

    //*****************************************************************************
    //
    // This example demonstrates how to send a string of data to the UART.
    //
    //*****************************************************************************
    int
    main(void)
    {
        uint32_t ui32Period;

        //
        // Set the clocking to run directly from the crystal at 120MHz.
        //
        g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                                 SYSCTL_OSC_MAIN |
                                                 SYSCTL_USE_PLL |
                                                 SYSCTL_CFG_VCO_480), 120000000);
        //
        // Enable the GPIO port that is used for the on-board LED.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
        //
        // Enable the GPIO pins for the LED (PN0).
        //
        GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0|GPIO_PIN_1);


        //
        // Enable the peripherals used by this example.
        //
        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);

        SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

        //
        // Enable processor interrupts.
        //
        IntMasterEnable();

            SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER3);
    //        TimerConfigure(TIMER3_BASE, TIMER_CFG_ONE_SHOT);
            TimerConfigure(TIMER3_BASE, TIMER_CFG_PERIODIC);


            ui32Period = g_ui32SysClock/2; // 1 ms one shot timer

    //        ui32Period = 5*g_ui32SysClock;
            TimerLoadSet(TIMER3_BASE, TIMER_A, ui32Period-1);

            IntEnable(INT_TIMER3A);
            TimerIntEnable(TIMER3_BASE, TIMER_TIMA_TIMEOUT);
            IntMasterEnable();

            TimerEnable(TIMER3_BASE, TIMER_A);


        //
        // Set GPIO A0 and A1 as UART pins.
        //
        GPIOPinConfigure(GPIO_PC6_U5RX);
        GPIOPinConfigure(GPIO_PC7_U5TX);
        GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);


        //
        // Configure the UART for 9600, 8-N-1 operation.
        //
        UARTConfigSetExpClk(UART5_BASE, g_ui32SysClock, 9600,
                                (UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
                                 UART_CONFIG_PAR_NONE));


        GPIOPinConfigure(GPIO_PA0_U0RX);
        GPIOPinConfigure(GPIO_PA1_U0TX);
        GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

        UARTStdioConfig(0, 9600, g_ui32SysClock);

        UART9BitAddrSet(UART5_BASE, 0x43, 0xFF);
        UART9BitEnable(UART5_BASE);


        UARTFIFODisable(UART5_BASE);

        //
        // Enable the UART interrupt.
        //
        IntEnable(INT_UART5);
        UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT | UART_INT_9BIT);
    //    ROM_UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT);
    //    ROM_UARTIntEnable(UART5_BASE, UART_INT_TX | UART_TXINT_MODE_EOT | UART_INT_9BIT);
    //    ROM_UARTIntEnable(UART5_BASE,UART_INT_TX|UART_TXINT_MODE_EOT | UART_INT_9BIT | UART_INT_RX|UART_INT_RT);

    //    UARTSend(TrxBuffer, 1);


    //    while(!(txcomplete));
        while(1);
    }

  • Use the past code </> option. The result is far more readable.

    Priya Nadathur70 said:
    I changed the LED blinking code to toggle without any delays. This made both EKs transmit correctly on timer interrupts. However receive uart in 9 bit mode is not working with either EK.

    Remember this?

     // Receive uart char
     while(ROM_UARTCharsAvail(UART5_BASE))
     {
     //
     // Read the next character from the UART and write it back to the UART.
     //
    
     UARTCharGet(UART5_BASE);
    
     }

    And here's the problem, you never deal with the other interrupts. Specifically you never deal with the 9-bit match receive interrupt. This, despite the fact that you enabled it.

    You still haven't dealt with it.

    Robert

  • I did this to receive on the 9 bit uart interrupt. Let me know if I should be doing something else:

    void

    UARTIntHandler(void)

    {

        uint32_t ui32Status;

        //

        // Get the interrrupt status.

        //

        ui32Status = UARTIntStatus(UART5_BASE, true);

        uint8_t interrupt_type = (uint8_t) ((ui32Status & 0x1000) >> 12);

        //

        //

        // Clear the asserted interrupts.

        //

        UARTIntClear(UART5_BASE, ui32Status);

        if (interrupt_type == 1){

            // Receive uart char

                 while(UARTCharsAvail(UART5_BASE))

                 {

                     //

                     // Read the next character from the UART and write it back to the UART.

                     //

                     UARTCharGet(UART5_BASE);

                 }

  • Pray tell, how does ignoring the issue help?

    Robert
  • I've been asked to amplify.

    Consider the following question:

    • What do you do when you receive any interrupt other than the one you are masking?
      • How do you detect it?
      • How do you respond to its occurrence?
        • Relatedly what do you expect from it?
      • How do you clear it?

    Related question:

    • What to expect when the UART receives a 9 bit 'character'?
      • What does the manual say?

    Robert