Hello,
Please answer below each question separately.
1> Is it possible to write 1-Bit data or 32-Bit Data to Parity RAM Area of NHET from CPU side when the HETPCR Register have TEST Bit set and PARITY_ENA=0x05?
2> Is it possible to write 1-Bit data or 32-Bit Data to Parity RAM Area of NHET from CPU side when the HETPCR Register have TEST Bit set and PARITY_ENA=0x0A?
3> Does HETGCR HET_ON Bit control in any way write access to NHET Parity RAM Area from CPU when TEST Bit of HETPCR is active?
Assume PENA bit is set so that NHET Peripheral is visible to CPU and active.
Thank you.
Regards
Pashan