Part Number: TMS570LC4357
Other Parts Discussed in Thread: UNIFLASH
Hey there,
we got a TMS570LC43 Launchpad for our project and we use an Lauterbach Power Debug Interface with Trace32 over Jtag to flash new software. The problem happend while flashing over Trace32, the power for the Board went low ( we mounted it on a RC-Car that runs with Battery) and the board went out. Now we cant access it anymore, nether with usb over Uniflash nor with the Lauterbach device.
If it is plugged in the 5V LED is on and nothing besides that. Not even the XDS110 status LEDs light up when we connect the USB.
The Lauterbach just prints that the device is in reset.
So is there any possible way to access the Launchpad again?
Thanks in advance for your answers
Philipp