Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN, TMS570LS1227
We are interested in using the SafeTI Diagnostic Library in our application with the TMS570LS0714. This MCU is listed as being supported by the library here
However, it is not listed as being supported in the Diagnostic Software Manual, SPNU592 (can't find a link). Is this simply because the manual, released January 2015 came out before the specific chip?
Overall, should we expect that the SafeTI functionality will work out of the box with the '0714? Also, do HALCoGen and the SafeTI diagnostic library integrate at all? In sys_startup and sys_selftest generated by HALCoGen, there seem to be functionality (such as PBIST) that should be covered by the diagnostic library. Is this just a case of HALCoGen calling SafeTI Diagnostic Library functions, or is it something else?