Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: EK-TM4C1294XL
Tool/software: Starterware
Hello.
Can anyone clear my doubts relating the eflash tool provided in the tools folder in Tivaware. I have read the bootloader document and it said that the the Tiva-C can be updated remotely via Ethernet connection. So i'm doing my hands on the eflash tool that is provided.
My doubt is what IP address do we need to specify in the " -i " parameter in the cmd file.
Also is it correct that a new image file can be sent via the internet and with the help of the eflash utility a new image can be flashed remotely from anywhere??
Also i have read in other posts that we need the boot_emac_flash code from the memory location 0x0 to enable the downloading of new image file using ethernet.
Thank you.