Part Number: EK-TM4C1294XL
Tool/software: TI-RTOS
I am continuing to troubleshoot a setup with two EK-TM4C1294XL.
Both EKs are set up to in 8 bit uart mode, interrupt on uart receive. I have the interrupts
for the uart and timer set up in the startup_ccs.c file.
EK1 sends a byte every 10 seconds, determined by a periodic timer. I have an LED set up
to blink when EK2 receives this byte. This LED toggles state once and not every 10 seconds
as expected. Why is the uart receive interrupt not repeatedly triggering? I have attached both
the transmitter and receiver EK files. On the scope, I can see the transmitted byte from EK1,
no byte visible on the scope from U5Rx on EK2.
Thanks,
Priya
EK1 transmitter:
//*****************************************************************************
//
// uart_echo.c - Example for reading data from and writing data to the UART in
// an interrupt driven fashion.
//
// Copyright (c) 2013-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.4.178 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/timer.h"
#include "utils/uartstdio.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>UART Echo (uart_echo)</h1>
//!
//! This example application utilizes the UART to echo text. The first UART
//! (connected to the USB debug virtual serial port on the evaluation board)
//! will be configured in 115,200 baud, 8-n-1 mode. All characters received on
//! the UART are transmitted back to the UART.
//
//*****************************************************************************
//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;
unsigned char txcomplete = 0;
unsigned char timerComplete = 0;
static uint8_t TrxBuffer[1] = {0x43};
uint8_t i = 0;
void UARTSend(const uint8_t *pui16Buffer, uint32_t ui32Count);
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
#endif
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
ROM_UARTCharPutNonBlocking(UART5_BASE, *pui8Buffer++);
}
}
//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = UARTIntStatus(UART5_BASE, true);
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART5_BASE, ui32Status);
if( ( (UART_INT_RX & ui32Status) == UART_INT_RX ) || ( (UART_INT_RT & ui32Status) == UART_INT_RT) ){
// Receive uart char
while(ROM_UARTCharsAvail(UART5_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
ROM_UARTCharGetNonBlocking(UART5_BASE);
//uint32_t c = UARTCharGet(UART5_BASE);
//
// Blink the LED to show a character transfer is occuring.
//
if(GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1))
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
}
else
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 2);
}
}
}
}
void Timer2IntHandler(void)
{
// Clear the timer interrupt
ROM_TimerIntClear(TIMER2_BASE, TIMER_TIMA_TIMEOUT);
i = 0;
UARTSend(TrxBuffer, 1);
// Blink the LED to show a character transfer is occuring.
//
if(GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1))
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
}
else
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 2);
}
timerComplete = 1;
}
//*****************************************************************************
//
// This example demonstrates how to send a string of data to the UART.
//
//*****************************************************************************
int
main(void)
{
uint32_t ui32Period;
//
// Set the clocking to run directly from the crystal at 120MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
//
// Enable the GPIO pins for the LED (PN0).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0|GPIO_PIN_1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER2);
ROM_IntMasterEnable();
//TimerConfigure(TIMER2_BASE, TIMER_CFG_ONE_SHOT);
ROM_TimerConfigure(TIMER2_BASE, TIMER_CFG_PERIODIC);
// ui32Period = g_ui32SysClock/200; // 5 ms one shot timer
ui32Period = 5*g_ui32SysClock;
// ui32Period = 3*g_ui32SysClock;
ROM_TimerLoadSet(TIMER2_BASE, TIMER_A, ui32Period);
ROM_IntEnable(INT_TIMER2A);
ROM_TimerIntEnable(TIMER2_BASE, TIMER_TIMA_TIMEOUT);
ROM_TimerEnable(TIMER2_BASE, TIMER_A);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Set GPIO A0 and A1 as UART pins.
//
ROM_GPIOPinConfigure(GPIO_PC6_U5RX);
ROM_GPIOPinConfigure(GPIO_PC7_U5TX);
ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
//
// Configure the UART for 9600, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART5_BASE, g_ui32SysClock, 9600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 9600, g_ui32SysClock);
// UART9BitAddrSet(UART5_BASE, 0x43, 0xFF);
// UART9BitEnable(UART5_BASE);
ROM_UARTEnable(UART5_BASE);
ROM_UARTFIFODisable(UART5_BASE);
// UART9BitAddrSend(UART5_BASE, 0x43);
//
// Enable the UART interrupt.
//
ROM_IntEnable(INT_UART5);
// UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT | UART_INT_9BIT);
ROM_UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT);
// ROM_UARTIntEnable(UART5_BASE, UART_INT_TX | UART_TXINT_MODE_EOT | UART_INT_9BIT);
// ROM_UARTIntEnable(UART5_BASE,UART_INT_TX|UART_TXINT_MODE_EOT | UART_INT_9BIT | UART_INT_RX|UART_INT_RT);
// UARTSend(TrxBuffer, 1);
// while(!(txcomplete));
while(1);
}
EK2 receiver:
//*****************************************************************************
//
// uart_echo.c - Example for reading data from and writing data to the UART in
// an interrupt driven fashion.
//
// Copyright (c) 2013-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.4.178 of the EK-TM4C1294XL Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/timer.h"
#include "utils/uartstdio.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>UART Echo (uart_echo)</h1>
//!
//! This example application utilizes the UART to echo text. The first UART
//! (connected to the USB debug virtual serial port on the evaluation board)
//! will be configured in 115,200 baud, 8-n-1 mode. All characters received on
//! the UART are transmitted back to the UART.
//
//*****************************************************************************
//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;
unsigned char txcomplete = 0;
unsigned char timerComplete = 0;
uint8_t TrxBuffer[1] = {0x21};
uint8_t i = 0;
void UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count);
void Timer3IntHandler(void);
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
ROM_UARTCharPutNonBlocking(UART5_BASE, *pui8Buffer++);
// UARTprintf("%x ", TrxBuffer[i++]);
}
}
void Timer3IntHandler(void)
{
// Clear the timer interrupt
ROM_TimerIntClear(TIMER3_BASE, TIMER_TIMA_TIMEOUT);
// Blink the LED to show a character transfer is occuring.
/*
if(GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1))
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
}
else
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 2);
}
*/
UARTSend(TrxBuffer, 1);
i = 0;
timerComplete = 1;
}
//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;
//
// Get the interrrupt status.
//
ui32Status = UARTIntStatus(UART5_BASE, true);
//
//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART5_BASE, ui32Status);
// if (interrupt_type == 1){
if( ( (UART_INT_RX & ui32Status) == UART_INT_RX ) || ( (UART_INT_RT & ui32Status) == UART_INT_RT) ){
// Receive uart char
while(ROM_UARTCharsAvail(UART5_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
// UARTCharPut(UART5_BASE, UARTCharGet(UART5_BASE));
ROM_UARTCharGetNonBlocking(UART5_BASE);
}
if(GPIOPinRead(GPIO_PORTN_BASE, GPIO_PIN_1))
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 0);
}
else
{
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_1, 2);
}
}
}
//*****************************************************************************
//
// This example demonstrates how to send a string of data to the UART.
//
//*****************************************************************************
int
main(void)
{
uint32_t ui32Period;
//
// Set the clocking to run directly from the crystal at 120MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
//
// Enable the GPIO pins for the LED (PN0).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0|GPIO_PIN_1);
//
// Enable the peripherals used by this example.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART5);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable processor interrupts.
//
ROM_IntMasterEnable();
#if 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER3);
// TimerConfigure(TIMER3_BASE, TIMER_CFG_ONE_SHOT);
TimerConfigure(TIMER3_BASE, TIMER_CFG_PERIODIC);
ui32Period = g_ui32SysClock/2; // 1 ms one shot timer
// ui32Period = 5*g_ui32SysClock;
TimerLoadSet(TIMER3_BASE, TIMER_A, ui32Period-1);
IntEnable(INT_TIMER3A);
TimerIntEnable(TIMER3_BASE, TIMER_TIMA_TIMEOUT);
IntMasterEnable();
TimerEnable(TIMER3_BASE, TIMER_A);
#endif
//
// Set GPIO A0 and A1 as UART pins.
//
ROM_GPIOPinConfigure(GPIO_PC6_U5RX);
ROM_GPIOPinConfigure(GPIO_PC7_U5TX);
ROM_GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7);
//
// Configure the UART for 9600, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART5_BASE, g_ui32SysClock, 9600,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTStdioConfig(0, 9600, g_ui32SysClock);
// UART9BitAddrSet(UART5_BASE, 0x43, 0xFF);
// UART9BitEnable(UART5_BASE);
ROM_UARTEnable(UART5_BASE);
ROM_UARTFIFODisable(UART5_BASE);
//
// Enable the UART interrupt.
//
ROM_IntEnable(INT_UART5);
// UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT | UART_INT_9BIT);
ROM_UARTIntEnable(UART5_BASE, UART_INT_RX | UART_INT_RT);
// ROM_UARTIntEnable(UART5_BASE, UART_INT_TX | UART_TXINT_MODE_EOT | UART_INT_9BIT);
// ROM_UARTIntEnable(UART5_BASE,UART_INT_TX|UART_TXINT_MODE_EOT | UART_INT_9BIT | UART_INT_RX|UART_INT_RT);
// UARTSend(TrxBuffer, 1);
// while(!(txcomplete));
while(1);
}
Thanks,
Priya