Hello,
If I use a 3.3V (+/- 2%) regulator for VDDA, will there be any adverse consequences to using a 3.3V (+/- 0.1%) VREFA+? In the worst-case scenario, I would have a difference of VREFA+ - VDDA = 3.3 * (1.001 - 0.98) = 69 mV. This is a small difference, but since the TM4C1294KCPDT datasheet lists the nominal and max value of VREFA+ as VDDA (pg 1859), I am curious if any negative impact on ADC performance would result.
I noticed that the design guide (pg 22) mentions using a 3.0V reference for VREFA+. However, I assume a larger VREFA+ is better since it slightly reduces the effect of noise and offset errors in the sensor and conditioning circuits.
For reference, here is what I am considering doing: