Part Number: TMS570LS1114
Other Parts Discussed in Thread: HALCOGEN
Hello:
I have two confused places when I use the ETPWM module.I want to implement 2ms control once ETPWM, and use the ETPWM module ADC Event trigger.But the ADC triggers the time control with the expected ETPWM frequency that can not be obtained at the same time.I do not know whether to use the RTI module to achieve, or use the HET module to achieve.HET can be accurate timing 2ms?Because I control the PWM at the same time need to use CAN every 5ms 15ms band to send the message.The second confusion is that I want to use ETPWM module TZn module, but when I open TZ1 TZ2 TZ3, the use of HALCoGen, my program will always be in a fault to judge, how to avoid it?Is my hardware design problem, or TZ1 TZ2 TZ3 failure mechanism can not always open it?
Looking forward to your reply
Qiu Chi