Other Parts Discussed in Thread: UNIFLASH,
Hello,
Before I started to flash my device with UniFlash I always used CCS to flash my devices. And that way I had no problems with my device.
Now I tried using Cloud UniFlash and tried to flash my device which has a TM4C1294NCPDT on it. The flashing tool that I used is XDS200 . First I flashed the device with hex file which i got from the CCS, the device did not start. After this I flashed the out file which the CCS generated, this time everything worked just fine only when I connected the device top my PC via USB, I could not read data from it and some information ware missing in the USB device description. When I read the USB description data I get this massage :
" Bus 001 Device 009: ID 1cbe:000a Luminary Micro Inc. Couldn't open device, some information will be missing " ***
After this I was thinking if I reflash my device with CCS everything will be okk but no, I get the same massage which i quoted.
After that I tried another board which had working firmware on it and the USB data sending was working, but this time I only read some registers like MAC address and device info, this was enough to render this bord useless.
Thanks for helping
Robert