Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL, SN65HVD230
Tool/software:Code Composer Studio
I tried running the following code for simple can communication as given in the examples.
Each time i press a key on the keyboard in order to transmit the same to another board, the values in CANIFnDAn registers changes according to the ASCII values
of the corresponding key pressed.
These are the following issues that i face.
1. The NEWDAT bit in the bit of the corresponding message in CANNWDAN register doesnt change even though the data
in the CANIFnDAN register changes with each key press.
2.TXOk bit in the CANSTS register doesn't change.
I need suggestions as to what could be the reason for the error or if i am missing any step
//*****************************************************************************
//
// can.c - Simple CAN example.
//
// Copyright (c) 2013-2016 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
//
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
//
// This is part of revision 2.1.3.156 of the DK-TM4C123G Firmware Package.
//
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_can.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/fpu.h"
#include "driverlib/can.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "grlib/grlib.h"
#include "drivers/cfal96x64x16.h"
#include "utils/uartstdio.h"
#include "driverlib/interrupt.h"
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>CAN Example (can)</h1>
//!
//! This example application utilizes CAN to send characters back and forth
//! between two boards. It uses the UART to read / write the characters to
//! the UART terminal. It also uses the graphical display on the board to show
//! the last character transmited / received. Error handling is also included.
//!
//! CAN HARDWARE SETUP:
//!
//! To use this example you will need to hook up two DK-TM4C123G boards
//! together in a CAN network. This involves hooking the CANH screw terminals
//! together and the CANL terminals together. In addition 120ohm termination
//! resistors will need to be added to the edges of the network between CANH
//! and CANL. In the two board setup this means hooking a 120 ohm resistor
//! between CANH and CANL on both boards.
//!
//! See diagram below for visual. '---' represents wire.
//!
//! \verbatim
//! CANH--+--------------------------+--CANH
//! | |
//! .-. .-.
//! | |120ohm | |120ohm
//! | | | |
//! '-' '-'
//! | |
//! CANL--+--------------------------+--CANL
//! \endverbatim
//!
//! SOFTWARE SETUP:
//!
//! Once the hardware connections are setup connect both boards to the computer
//! via the In-Circuit Debug Interface USB port next to the graphical display.
//! Attach a UART terminal to each board configured 115,200 baud, 8-n-1 mode.
//!
//! Anything you type into one terminal will show up in the other terminal and
//! vice versa. The last character sent / received will also be displayed on
//! the graphical display on the board.
//
//*****************************************************************************
//*****************************************************************************
//
// A counter that keeps track of the number of times the TX & RX interrupt has
// occurred, which should match the number of messages that were transmitted /
// received.
//
//*****************************************************************************
volatile uint32_t g_ui32RXMsgCount = 0;
volatile uint32_t g_ui32TXMsgCount = 0;
//*****************************************************************************
//
// A flag for the interrupt handler to indicate that a message was received.
//
//*****************************************************************************
volatile bool g_bRXFlag = 0;
//*****************************************************************************
//
// A global to keep track of the error flags that have been thrown so they may
// be processed. This is necessary because reading the error register clears
// the flags, so it is necessary to save them somewhere for processing.
//
//*****************************************************************************
volatile uint32_t g_ui32ErrFlag = 0;
//*****************************************************************************
//
// CAN message Objects for data being sent / received
//
//*****************************************************************************
tCANMsgObject g_sCAN0RxMessage;
tCANMsgObject g_sCAN0TxMessage;
//*****************************************************************************
//
// Message Identifiers and Objects
// RXID is set to 0 so all messages are received
//
//*****************************************************************************
#define CAN0RXID 0
#define RXOBJECT 1
#define CAN0TXID 2
#define TXOBJECT 2
//*****************************************************************************
//
// Variables to hold character being sent / reveived
//
//*****************************************************************************
uint8_t g_ui8TXMsgData;
uint8_t g_ui8RXMsgData;
//*****************************************************************************
//
// Global context for text printed on graphics display
//
//*****************************************************************************
tContext g_sContext;
//*****************************************************************************
//
// Screen line deffinitions, offsets from top in pixels
//
//*****************************************************************************
#define SCREENLINE1 10
#define SCREENLINE2 20
#define SCREENLINE3 30
#define SCREENLINE4 40
#define SCREENLINE5 50
//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif
//*****************************************************************************
//
// CAN 0 Interrupt Handler. It checks for the cause of the interrupt, and
// maintains a count of all messages that have been transmitted / received
//
//*****************************************************************************
void
CAN0IntHandler(void)
{
uint32_t ui32Status;
//
// Read the CAN interrupt status to find the cause of the interrupt
//
// CAN_INT_STS_CAUSE register values
// 0x0000 = No Interrupt Pending
// 0x0001-0x0020 = Number of message object that caused the interrupt
// 0x8000 = Status interrupt
// all other numbers are reserved and have no meaning in this system
//
ui32Status = CANIntStatus(CAN0_BASE, CAN_INT_STS_CAUSE);
//
// If this was a status interrupt acknowledge it by reading the CAN
// controller status register.
//
if(ui32Status == CAN_INT_INTID_STATUS)
{
//
// Read the controller status. This will return a field of status
// error bits that can indicate various errors. Refer to the
// API documentation for details about the error status bits.
// The act of reading this status will clear the interrupt.
//
ui32Status = CANStatusGet(CAN0_BASE, CAN_STS_CONTROL);
//
// Add ERROR flags to list of current errors. To be handled
// later, because it would take too much time here in the
// interrupt.
//
g_ui32ErrFlag |= ui32Status;
}
//
// Check if the cause is message object RXOBJECT, which we are using
// for receiving messages.
//
else if(ui32Status == RXOBJECT)
{
//
// Getting to this point means that the RX interrupt occurred on
// message object RXOBJECT, and the message reception is complete.
// Clear the message object interrupt.
//
CANIntClear(CAN0_BASE, RXOBJECT);
//
// Increment a counter to keep track of how many messages have been
// received. In a real application this could be used to set flags to
// indicate when a message is received.
//
g_ui32RXMsgCount++;
//
// Set flag to indicate received message is pending.
//
g_bRXFlag = true;
//
// Since a message was received, clear any error flags.
// This is done because before the message is received it triggers
// a Status Interrupt for RX complete. by clearing the flag here we
// prevent unnecessary error handling from happeneing
//
g_ui32ErrFlag = 0;
}
//
// Check if the cause is message object TXOBJECT, which we are using
// for transmitting messages.
//
else if(ui32Status == TXOBJECT)
{
//
// Getting to this point means that the TX interrupt occurred on
// message object TXOBJECT, and the message reception is complete.
// Clear the message object interrupt.
//
CANIntClear(CAN0_BASE, TXOBJECT);
//
// Increment a counter to keep track of how many messages have been
// transmitted. In a real application this could be used to set
// flags to indicate when a message is transmitted.
//
g_ui32TXMsgCount++;
//
// Since a message was transmitted, clear any error flags.
// This is done because before the message is transmitted it triggers
// a Status Interrupt for TX complete. by clearing the flag here we
// prevent unnecessary error handling from happeneing
//
g_ui32ErrFlag = 0;
}
//
// Otherwise, something unexpected caused the interrupt. This should
// never happen.
//
else
{
//
// Spurious interrupt handling can go here.
//
}
}
//*****************************************************************************
//
// Configure the UART and its pins. This must be called before UARTprintf().
//
//*****************************************************************************
void
ConfigureUART(void)
{
//
// Enable the GPIO Peripheral used by the UART.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Enable UART0
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Configure GPIO Pins for UART mode.
//
ROM_GPIOPinConfigure(GPIO_PA0_U0RX);
ROM_GPIOPinConfigure(GPIO_PA1_U0TX);
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// Setup CAN0 to both send and receive at 500KHz.
// Interrupts on
// Use PE4 / PE5
//
//*****************************************************************************
void
InitCAN0(void)
{
//
// For this example CAN0 is used with RX and TX pins on port E4 and E5.
// GPIO port E needs to be enabled so these pins can be used.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Configure the GPIO pin muxing to select CAN0 functions for these pins.
// This step selects which alternate function is available for these pins.
//
GPIOPinConfigure(GPIO_PB4_CAN0RX);
GPIOPinConfigure(GPIO_PB5_CAN0TX);
//
// Enable the alternate function on the GPIO pins. The above step selects
// which alternate function is available. This step actually enables the
// alternate function instead of GPIO for these pins.
//
GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
//
// The GPIO port and pins have been set up for CAN. The CAN peripheral
// must be enabled.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
//
// Initialize the CAN controller
//
CANInit(CAN0_BASE);
//
// Set up the bit rate for the CAN bus. This function sets up the CAN
// bus timing for a nominal configuration. You can achieve more control
// over the CAN bus timing by using the function CANBitTimingSet() instead
// of this one, if needed.
// In this example, the CAN bus is set to 500 kHz.
//
CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
//
// Enable interrupts on the CAN peripheral. This example uses static
// allocation of interrupt handlers which means the name of the handler
// is in the vector table of startup code.
//
CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
//
// Enable the CAN interrupt on the processor (NVIC).
//
IntEnable(INT_CAN0);
//
// Enable the CAN for operation.
//
CANEnable(CAN0_BASE);
//
// Initialize a message object to be used for receiving CAN messages with
// any CAN ID. In order to receive any CAN ID, the ID and mask must both
// be set to 0, and the ID filter enabled.
//
g_sCAN0RxMessage.ui32MsgID = CAN0RXID;
g_sCAN0RxMessage.ui32MsgIDMask = 0;
g_sCAN0RxMessage.ui32Flags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER;
g_sCAN0RxMessage.ui32MsgLen = sizeof(g_ui8RXMsgData);
//
// Now load the message object into the CAN peripheral. Once loaded the
// CAN will receive any message on the bus, and an interrupt will occur.
// Use message object RXOBJECT for receiving messages (this is not the
//same as the CAN ID which can be any value in this example).
//
CANMessageSet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, MSG_OBJ_TYPE_RX);
//
// Initialize the message object that will be used for sending CAN
// messages. The message will be 1 bytes that will contain the character
// received from the other controller. Initially it will be set to 0.
//
g_ui8TXMsgData = 0;
g_sCAN0TxMessage.ui32MsgID = CAN0TXID;
g_sCAN0TxMessage.ui32MsgIDMask = 0;
g_sCAN0TxMessage.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
g_sCAN0TxMessage.ui32MsgLen = sizeof(g_ui8TXMsgData);
g_sCAN0TxMessage.pui8MsgData = (uint8_t *)&g_ui8TXMsgData;
}
//*****************************************************************************
//
// Set up the OLED Graphical Display
//
//*****************************************************************************
void
InitGraphics(void)
{
tRectangle sRect;
//
// Initialize the display driver.
//
CFAL96x64x16Init();
//
// Initialize the graphics context.
//
GrContextInit(&g_sContext, &g_sCFAL96x64x16);
//
// Fill the top 24 rows of the screen with blue to create the banner.
//
sRect.i16XMin = 0;
sRect.i16YMin = 0;
sRect.i16XMax = GrContextDpyWidthGet(&g_sContext) - 1;
sRect.i16YMax = 9;
GrContextForegroundSet(&g_sContext, ClrDarkBlue);
GrRectFill(&g_sContext, &sRect);
//
// Put a white box around the banner.
//
GrContextForegroundSet(&g_sContext, ClrWhite);
GrRectDraw(&g_sContext, &sRect);
//
// Put the application name in the middle of the banner.
//
GrContextFontSet(&g_sContext, g_psFontFixed6x8);
GrStringDrawCentered(&g_sContext, "CAN Example", -1,
GrContextDpyWidthGet(&g_sContext) / 2, 4, 0);
//
// Flush any cached drawing operations.
//
GrFlush(&g_sContext);
}
//*****************************************************************************
//
// Can ERROR handling. When a message is received if there is an erro it is
// saved to g_ui32ErrFlag, the Error Flag Set. Below the flags are checked
// and cleared. It is left up to the user to add handling fuctionality if so
// desiered.
//
// For more information on the error flags please see the CAN section of the
// microcontroller datasheet.
//
// NOTE: you may experience errors during setup when only one board is powered
// on. This is caused by one board sending signals and there not being another
// board there to acknoledge it. Dont worry about these errors, they can be
// disregarded.
//
//*****************************************************************************
void
CANErrorHandler(void)
{
//
// CAN controller has entered a Bus Off state.
//
if(g_ui32ErrFlag & CAN_STATUS_BUS_OFF)
{
//
// Handle Error Condition here
//
UARTprintf(" ERROR: CAN_STATUS_BUS_OFF \n");
//
// Clear CAN_STATUS_BUS_OFF Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_BUS_OFF);
}
//
// CAN controller error level has reached warning level.
//
if(g_ui32ErrFlag & CAN_STATUS_EWARN)
{
//
// Handle Error Condition here
//
//UARTprintf(" ERROR: CAN_STATUS_EWARN \n");
//
// Clear CAN_STATUS_EWARN Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_EWARN);
}
//
// CAN controller error level has reached error passive level.
//
if(g_ui32ErrFlag & CAN_STATUS_EPASS)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_EPASS Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_EPASS);
}
//
// A message was received successfully since the last read of this status.
//
if(g_ui32ErrFlag & CAN_STATUS_RXOK)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_RXOK Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_RXOK);
}
//
// A message was transmitted successfully since the last read of this
// status.
//
if(g_ui32ErrFlag & CAN_STATUS_TXOK)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_TXOK Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_TXOK);
}
//
// This is the mask for the last error code field.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_MSK)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_MSK Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_MSK);
}
//
// A bit stuffing error has occurred.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_STUFF)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_STUFF Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_STUFF);
}
//
// A formatting error has occurred.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_FORM)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_FORM Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_FORM);
}
//
// An acknowledge error has occurred.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_ACK)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_ACK Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_ACK);
}
//
// The bus remained a bit level of 1 for longer than is allowed.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_BIT1)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_BIT1 Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_BIT1);
}
//
// The bus remained a bit level of 0 for longer than is allowed.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_BIT0)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_BIT0 Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_BIT0);
}
//
// A CRC error has occurred.
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_CRC)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_CRC Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_CRC);
}
//
// This is the mask for the CAN Last Error Code (LEC).
//
if(g_ui32ErrFlag & CAN_STATUS_LEC_MASK)
{
//
// Handle Error Condition here
//
//
// Clear CAN_STATUS_LEC_MASK Flag
//
g_ui32ErrFlag &= ~(CAN_STATUS_LEC_MASK);
}
//
// If there are any bits still set in g_ui32ErrFlag then something unhandled
// has happened. Print the value of g_ui32ErrFlag.
//
if(g_ui32ErrFlag !=0)
{
UARTprintf(" Unhandled ERROR: %x \n",g_ui32ErrFlag);
}
}
//*****************************************************************************
//
// Set up the system, initialize the UART, Graphics, and CAN. Then poll the
// UART for data. If there is any data send it, if there is any thing received
// print it out to the UART. If there are errors call the error handling
// function.
//
//*****************************************************************************
int
main(void)
{
//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
ROM_FPULazyStackingEnable();
//
// Set the clocking to run directly from the crystal.
//
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
//
// Initialize the UART
//
ConfigureUART();
//
// Initialize CAN0
//
InitCAN0();
//
// Print welcome message
//
UARTprintf("\nCAN Example App\n");
UARTprintf("Type something to see it show up on the other terminal: \n\n");
//
// Poll UART for data, transmit across CAN when something is entered
//
while(1)
{
//
// If the flag is set, that means that the RX interrupt occurred and
// there is a message ready to be read from the CAN
//
if(g_bRXFlag)
{
//
// Reuse the same message object that was used earlier to configure
// the CAN for receiving messages. A buffer for storing the
// received data must also be provided, so set the buffer pointer
// within the message object.
//
g_sCAN0RxMessage.pui8MsgData = (uint8_t *) &g_ui8RXMsgData;
//
// Read the message from the CAN. Message object RXOBJECT is used
// (which is not the same thing as CAN ID). The interrupt clearing
// flag is not set because this interrupt was already cleared in
// the interrupt handler.
//
CANMessageGet(CAN0_BASE, RXOBJECT, &g_sCAN0RxMessage, 0);
//
// Clear the pending message flag so that the interrupt handler can
// set it again when the next message arrives.
//
g_bRXFlag = 0;
//
// Check to see if there is an indication that some messages were
// lost.
//
if(g_sCAN0RxMessage.ui32Flags & MSG_OBJ_DATA_LOST)
{
UARTprintf("\nCAN message loss detected\n");
}
//
// Print the received character to the UART terminal
//
UARTprintf("%c", g_ui8RXMsgData);
}
else
{
//
// Error Handling
//
if(g_ui32ErrFlag != 0)
{
CANErrorHandler();
}
//
// See if there is something new to transmit
//
while(ROM_UARTCharsAvail(UART0_BASE))
{
//
// Read the next character from the UART terminal
//
g_ui8TXMsgData = ROM_UARTCharGetNonBlocking(UART0_BASE);
//
// Send the CAN message using object number TXOBJECT (not the
// same thing as CAN ID, which is also TXOBJECT in this
// example). This function will cause the message to be
// transmitted right away.
//
CANMessageSet(CAN0_BASE, TXOBJECT, &g_sCAN0TxMessage,
MSG_OBJ_TYPE_TX);
}
}
}
}