Tool/software: Code Composer Studio
Hello,
I am using the TMS570LS1114PGE EEPROM module,HALCoGen generating Code,but I have two questions.
1. My computer is the CCS installation directory on the D drive, according to the HAL to find, and did not find F021_API_CortexR4_BE_V3D16 this path. with
Path C: / ti / Hercules / F021 Flash API / 2.01.01 / include to Include Path in CCS Project
what should I do?
2.Do I need to write these important configuration addresses to EEPROM when I write some important configuration into the EEPROM?
Looking forward to your replay
Qiu Chi