Part Number: EK-TM4C1294XL
I am trying to dubug the following code for CAN Tx side. I have connected the EK-TM4C1294XL board to PC using USB and using putty to view the results though the UART.
The code I am running is the following:
//*****************************************************************************
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_can.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/can.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
#include "utils/uartstdio.c"
//*****************************************************************************
//
//! \addtogroup can_examples_list
//! <h1>Multiple CAN TX (multi_tx)</h1>
//!
//! This example shows how to set up the CAN to send multiple messages. The
//! CAN peripheral is configured to send messages with 4 different CAN IDs.
//! Two of the messages (with different CAN IDs) are sent using a shared
//! message object. This shows how to reuse a message object for multiple
//! messages. The other two messages are sent using their own message objects.
//! All four messages are transmitted once per second. The content of each
//! message is a test pattern. A CAN interrupt handler is used to confirm
//! message transmission and count the number of messages that have been sent.
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - CAN1 peripheral
//! - GPIO Port B peripheral (for CAN1 pins)
//! - CAN1RX - PB0
//! - CAN1TX - PB1
//!
//! The following UART signals are configured only for displaying console
//! messages for this example. These are not required for operation of CAN.
//! - GPIO port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - INT_CAN1 - CANIntHandler
//
//*****************************************************************************
//*****************************************************************************
//
// A counter that keeps track of the number of times the TX interrupt has
// occurred, which should match the number of TX messages that were sent.
//
//*****************************************************************************
volatile uint32_t g_ui32IntCount = 0;
//*****************************************************************************
//
// Counters that are used to count the number of messages on each of the
// three message objects that are used in this example.
//
//*****************************************************************************
volatile uint32_t g_ui32Msg1Count = 0;
volatile uint32_t g_ui32Msg2Count = 0;
volatile uint32_t g_ui32Msg3Count = 0;
//*****************************************************************************
//
// A flag to indicate that CAN controller message object 3 has sent a message.
//
//*****************************************************************************
volatile bool g_bMsgObj3Sent = 0;
//*****************************************************************************
//
// A flag to indicate that some transmission error occurred.
//
//*****************************************************************************
volatile bool g_bErrFlag = 0;
//*****************************************************************************
//
// CAN message objects that will hold the separate CAN messages. These could
// also be allocated on the stack but be careful because these structures
// each take about 20 bytes.
//
//*****************************************************************************
tCANMsgObject g_sCANMsgObject1;
tCANMsgObject g_sCANMsgObject2;
tCANMsgObject g_sCANMsgObject3;
//*****************************************************************************
//
// Message buffers that hold the contents of the 4 different messages that
// are being transmitted. Each one is a different length.
//
//*****************************************************************************
uint8_t g_pui8Msg1[4] = { 1, 3, 5, 7 };
uint8_t g_pui8Msg2[5] = { 2, 4, 6, 8, 10 };
uint8_t g_pui8Msg3[6] = { 3, 6, 9, 12, 15, 18 };
uint8_t g_pui8Msg4[8] = { 4, 8, 12, 16, 20, 24, 28, 32 };
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void
InitConsole(void)
{
//
// Enable GPIO port A which is used for UART0 pins.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Configure the pin muxing for UART0 functions on port A0 and A1.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
//
// Enable UART0 so that we can configure the clock.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Select the alternate (UART) function for these pins.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// This function prints some information about the CAN message to the
// serial port for information purposes only.
//
//*****************************************************************************
void
PrintCANMessageInfo(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj)
{
unsigned int uIdx;
UARTprintf("Sending msg: obj=%d ID=0x%04X msg=0x", ui32MsgObj,
psCANMsg->ui32MsgID);
for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++)
{
UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]);
}
UARTprintf("\n");
}
//*****************************************************************************
//
// This function provides a 1 second delay using a simple polling method.
//
//*****************************************************************************
void
SimpleDelay(void)
{
//
// Delay cycles for 1 second
//
SysCtlDelay(16000000 / 3);
}
//*****************************************************************************
//
// This function is the interrupt handler for the CAN peripheral. It checks
// for the cause of the interrupt, and maintains a count of all messages that
// have been transmitted.
//
//*****************************************************************************
void
CANIntHandler(void)
{
uint32_t ui32Status;
//
// Read the CAN interrupt status to find the cause of the interrupt
//
ui32Status = CANIntStatus(CAN1_BASE, CAN_INT_STS_CAUSE);
//
// If the cause is a controller status interrupt, then get the status
//
if(ui32Status == CAN_INT_INTID_STATUS)
{
//
// Read the controller status. This will return a field of status
// error bits that can indicate various errors. Error processing
// is not done in this example for simplicity. Refer to the
// API documentation for details about the error status bits.
// The act of reading this status will clear the interrupt. If the
// CAN peripheral is not connected to a CAN bus with other CAN devices
// present, then errors will occur and will be indicated in the
// controller status.
//
ui32Status = CANStatusGet(CAN1_BASE, CAN_STS_CONTROL);
//
// Set a flag to indicate some errors may have occurred.
//
g_bErrFlag = 1;
}
//
// Check if the cause is message object 1, which is used for sending
// message 1.
//
else if(ui32Status == 1)
{
//
// Getting to this point means that the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
//
CANIntClear(CAN1_BASE, 1);
//
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
//
g_ui32Msg1Count++;
//
// Since the message was sent, clear any error flags.
//
g_bErrFlag = 0;
}
//
// Check if the cause is message object 2, which is used for sending
// message 2.
//
else if(ui32Status == 2)
{
//
// Getting to this point means that the TX interrupt occurred on
// message object 2, and the message TX is complete. Clear the
// message object interrupt.
//
CANIntClear(CAN1_BASE, 2);
//
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
//
g_ui32Msg2Count++;
//
// Since the message was sent, clear any error flags.
//
g_bErrFlag = 0;
}
//
// Check if the cause is message object 3, which is used for sending
// messages 3 and 4.
//
else if(ui32Status == 3)
{
//
// Getting to this point means that the TX interrupt occurred on
// message object 3, and a message TX is complete. Clear the
// message object interrupt.
//
CANIntClear(CAN1_BASE, 3);
//
// Increment a counter to keep track of how many messages have been
// sent. In a real application this could be used to set flags to
// indicate when a message is sent.
//
g_ui32Msg3Count++;
//
// Set the flag indicating that a message was sent using message
// object 3. The program main loop uses this to know when to send
// another message using message object 3.
//
g_bMsgObj3Sent = 1;
//
// Since the message was sent, clear any error flags.
//
g_bErrFlag = 0;
}
//
// Otherwise, something unexpected caused the interrupt. This should
// never happen.
//
else
{
//
// Spurious interrupt handling can go here.
//
}
}
//*****************************************************************************
//
// Configure the CAN and enter a loop to transmit periodic CAN messages.
//
//*****************************************************************************
int
main(void)
{
uint32_t ui32SysClock;
ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_INT |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Set up the serial console to use for displaying messages. This is
// just for this example program and is not needed for CAN operation.
//
InitConsole();
//
// For this example CAN1 is used with RX and TX pins on port B4 and B5.
// The actual port and pins used may be different on your part, consult
// the data sheet for more information.
// GPIO port B needs to be enabled so these pins can be used.
// TODO: change this to whichever GPIO port you are using
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//
// Configure the GPIO pin muxing to select CAN1 functions for these pins.
// This step selects which alternate function is available for these pins.
// This is necessary if your part supports GPIO pin function muxing.
// Consult the data sheet to see which functions are allocated per pin.
// TODO: change this to select the port/pin you are using
//
GPIOPinConfigure(GPIO_PB0_CAN1RX);
GPIOPinConfigure(GPIO_PB1_CAN1TX);
//
// Enable the alternate function on the GPIO pins. The above step selects
// which alternate function is available. This step actually enables the
// alternate function instead of GPIO for these pins.
// TODO: change this to match the port/pin you are using
//
GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// The GPIO port and pins have been set up for CAN. The CAN peripheral
// must be enabled.
//
SysCtlPeripheralDisable(SYSCTL_PERIPH_CAN1);
SysCtlPeripheralReset(SYSCTL_PERIPH_CAN1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN1);
//
// Initialize the CAN controller
//
CANInit(CAN1_BASE);
//
// Set up the bit rate for the CAN bus. This function sets up the CAN
// bus timing for a nominal configuration. You can achieve more control
// over the CAN bus timing by using the function CANBitTimingSet() instead
// of this one, if needed.
// In this example, the CAN bus is set to 500 kHz. In the function below,
// the call to SysCtlClockGet() is used to determine the clock rate that
// is used for clocking the CAN peripheral. This can be replaced with a
// fixed value if you know the value of the system clock, saving the extra
// function call. For some parts, the CAN peripheral is clocked by a fixed
// 8 MHz regardless of the system clock in which case the call to
// SysCtlClockGet() should be replaced with 8000000. Consult the data
// sheet for more information about CAN peripheral clocking.
//
CANBitRateSet(CAN1_BASE, ui32SysClock, 500000);
//
// Enable interrupts on the CAN peripheral. This example uses static
// allocation of interrupt handlers which means the name of the handler
// is in the vector table of startup code. If you want to use dynamic
// allocation of the vector table, then you must also call CANIntRegister()
// here.
//
CANIntRegister(CAN1_BASE, CANIntHandler); // if using dynamic vectors
//
CANIntEnable(CAN1_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
//
// Enable the CAN interrupt on the processor (NVIC).
//
IntEnable(INT_CAN1);
//
// Enable the CAN for operation.
//
CANEnable(CAN1_BASE);
//
// Initialize the message object that will be used for sending CAN
// messages. The message will be 4 bytes that will contain an incrementing
// value. Initially it will be set to 0.
//
//
// Initialize message object 1 to be able to send CAN message 1. This
// message object is not shared so it only needs to be initialized one
// time, and can be used for repeatedly sending the same message ID.
//
g_sCANMsgObject1.ui32MsgID = 0x1001;
g_sCANMsgObject1.ui32MsgIDMask = 0;
g_sCANMsgObject1.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
g_sCANMsgObject1.ui32MsgLen = sizeof(g_pui8Msg1);
g_sCANMsgObject1.pui8MsgData = g_pui8Msg1;
//
// Initialize message object 2 to be able to send CAN message 2. This
// message object is not shared so it only needs to be initialized one
// time, and can be used for repeatedly sending the same message ID.
//
g_sCANMsgObject2.ui32MsgID = 0x2001;
g_sCANMsgObject2.ui32MsgIDMask = 0;
g_sCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
g_sCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg2);
g_sCANMsgObject2.pui8MsgData = g_pui8Msg2;
//
// Enter loop to send messages. Four messages will be sent once per
// second. The contents of each message will be changed each time.
//
for(;;)
{
//
// Send message 1 using CAN controller message object 1. This is
// the only message sent using this message object. The
// CANMessageSet() function will cause the message to be sent right
// away.
//
PrintCANMessageInfo(&g_sCANMsgObject1, 1);
CANMessageSet(CAN1_BASE, 1, &g_sCANMsgObject1, MSG_OBJ_TYPE_TX);
UARTprintf("%d\n",g_ui32Msg1Count);
//
// Send message 2 using CAN controller message object 2. This is
// the only message sent using this message object. The
// CANMessageSet() function will cause the message to be sent right
// away.
//
PrintCANMessageInfo(&g_sCANMsgObject2, 2);
CANMessageSet(CAN1_BASE, 2, &g_sCANMsgObject2, MSG_OBJ_TYPE_TX);
UARTprintf("%d\n",g_ui32Msg2Count);
//
// Load message object 3 with message 3. This is needs to be done each
// time because message object 3 is being shared for two different
// messages.
//
g_sCANMsgObject3.ui32MsgID = 0x3001;
g_sCANMsgObject3.ui32MsgIDMask = 0;
g_sCANMsgObject3.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
g_sCANMsgObject3.ui32MsgLen = sizeof(g_pui8Msg3);
g_sCANMsgObject3.pui8MsgData = g_pui8Msg3;
//
// Clear the flag that indicates that message 3 has been sent. This
// flag will be set in the interrupt handler when a message has been
// sent using message object 3.
//
g_bMsgObj3Sent = 0;
//
// Now send message 3 using CAN controller message object 3. This is
// the first message sent using this message object. The
// CANMessageSet() function will cause the message to be sent right
// away.
//
PrintCANMessageInfo(&g_sCANMsgObject3, 3);
CANMessageSet(CAN1_BASE, 3, &g_sCANMsgObject3, MSG_OBJ_TYPE_TX);
//
// Wait for the indication from the interrupt handler that message
// object 3 is done, because we are re-using it for another message.
//
while(!g_bMsgObj3Sent)
{
}
UARTprintf("%d\n",g_ui32Msg3Count);
//
// Load message object 3 with message 4. This is needed because
// message object 3 is being shared for two different messages.
//
g_sCANMsgObject3.ui32MsgID = 0x3002;
g_sCANMsgObject3.ui32MsgIDMask = 0;
g_sCANMsgObject3.ui32Flags = MSG_OBJ_TX_INT_ENABLE;
g_sCANMsgObject3.ui32MsgLen = sizeof(g_pui8Msg4);
g_sCANMsgObject3.pui8MsgData = g_pui8Msg4;
//
// Now send message 4 using CAN controller message object 3. This is
// the second message sent using this message object. The
// CANMessageSet() function will cause the message to be sent right
// away.
//
PrintCANMessageInfo(&g_sCANMsgObject3, 3);
CANMessageSet(CAN1_BASE, 3, &g_sCANMsgObject3, MSG_OBJ_TYPE_TX);
}
//
// Return no errors
//
//return(0);
}
The result of the above code is:
Please note the lines in red coloured font in the code.
The above in putty is received when the UARTprintf("%d\n",g_ui32Msg3Count); is included after while(!g_bMsgObj3Sent) { }
But if I include the UARTprintf("%d\n",g_ui32Msg3Count) before while(!g_bMsgObj3Sent) { } I am getting the below shown result in putty:
So the program execution seems to be stuck in the while loop: while(!g_bMsgObj3Sent) { }
The program is designed to reuse the message object to send multiple data.
Is there any remedy ?
//*****************************************************************************//// multi_tx.c - Peripheral example demonstrating multiple CAN message// transmission.//// Copyright (c) 2010-2014 Texas Instruments Incorporated. All rights reserved.// Software License Agreement//// Redistribution and use in source and binary forms, with or without// modification, are permitted provided that the following conditions// are met://// Redistributions of source code must retain the above copyright// notice, this list of conditions and the following disclaimer.//// Redistributions in binary form must reproduce the above copyright// notice, this list of conditions and the following disclaimer in the// documentation and/or other materials provided with the// distribution.//// Neither the name of Texas Instruments Incorporated nor the names of// its contributors may be used to endorse or promote products derived// from this software without specific prior written permission.//// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.//// This is part of revision 2.1.0.12573 of the Tiva Firmware Development Package.////*****************************************************************************
#include <stdbool.h>#include <stdint.h>#include "inc/hw_can.h"#include "inc/hw_ints.h"#include "inc/hw_memmap.h"#include "driverlib/can.h"#include "driverlib/gpio.h"#include "driverlib/interrupt.h"#include "driverlib/pin_map.h"#include "driverlib/sysctl.h"#include "driverlib/uart.h"#include "utils/uartstdio.h"#include "utils/uartstdio.c"
//*****************************************************************************////! \addtogroup can_examples_list//! <h1>Multiple CAN TX (multi_tx)</h1>//!//! This example shows how to set up the CAN to send multiple messages. The//! CAN peripheral is configured to send messages with 4 different CAN IDs.//! Two of the messages (with different CAN IDs) are sent using a shared//! message object. This shows how to reuse a message object for multiple//! messages. The other two messages are sent using their own message objects.//! All four messages are transmitted once per second. The content of each//! message is a test pattern. A CAN interrupt handler is used to confirm//! message transmission and count the number of messages that have been sent.//!//! This example uses the following peripherals and I/O signals. You must//! review these and change as needed for your own board://! - CAN1 peripheral//! - GPIO Port B peripheral (for CAN1 pins)//! - CAN1RX - PB0//! - CAN1TX - PB1//!//! The following UART signals are configured only for displaying console//! messages for this example. These are not required for operation of CAN.//! - GPIO port A peripheral (for UART0 pins)//! - UART0RX - PA0//! - UART0TX - PA1//!//! This example uses the following interrupt handlers. To use this example//! in your own application you must add these interrupt handlers to your//! vector table.//! - INT_CAN1 - CANIntHandler////*****************************************************************************
//*****************************************************************************//// A counter that keeps track of the number of times the TX interrupt has// occurred, which should match the number of TX messages that were sent.////*****************************************************************************volatile uint32_t g_ui32IntCount = 0;
//*****************************************************************************//// Counters that are used to count the number of messages on each of the// three message objects that are used in this example.////*****************************************************************************volatile uint32_t g_ui32Msg1Count = 0;volatile uint32_t g_ui32Msg2Count = 0;volatile uint32_t g_ui32Msg3Count = 0;
//*****************************************************************************//// A flag to indicate that CAN controller message object 3 has sent a message.////*****************************************************************************volatile bool g_bMsgObj3Sent = 0;
//*****************************************************************************//// A flag to indicate that some transmission error occurred.////*****************************************************************************volatile bool g_bErrFlag = 0;
//*****************************************************************************//// CAN message objects that will hold the separate CAN messages. These could// also be allocated on the stack but be careful because these structures// each take about 20 bytes.////*****************************************************************************tCANMsgObject g_sCANMsgObject1;tCANMsgObject g_sCANMsgObject2;tCANMsgObject g_sCANMsgObject3;
//*****************************************************************************//// Message buffers that hold the contents of the 4 different messages that// are being transmitted. Each one is a different length.////*****************************************************************************uint8_t g_pui8Msg1[4] = { 1, 3, 5, 7 };uint8_t g_pui8Msg2[5] = { 2, 4, 6, 8, 10 };uint8_t g_pui8Msg3[6] = { 3, 6, 9, 12, 15, 18 };uint8_t g_pui8Msg4[8] = { 4, 8, 12, 16, 20, 24, 28, 32 };
//*****************************************************************************//// This function sets up UART0 to be used for a console to display information// as the example is running.////*****************************************************************************voidInitConsole(void){ // // Enable GPIO port A which is used for UART0 pins. // TODO: change this to whichever GPIO port you are using. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
// // Configure the pin muxing for UART0 functions on port A0 and A1. // This step is not necessary if your part does not support pin muxing. // TODO: change this to select the port/pin you are using. // GPIOPinConfigure(GPIO_PA0_U0RX); GPIOPinConfigure(GPIO_PA1_U0TX);
// // Enable UART0 so that we can configure the clock. // SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
// // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
// // Select the alternate (UART) function for these pins. // TODO: change this to select the port/pin you are using. // GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
// // Initialize the UART for console I/O. // UARTStdioConfig(0, 115200, 16000000);}
//*****************************************************************************//// This function prints some information about the CAN message to the// serial port for information purposes only.////*****************************************************************************voidPrintCANMessageInfo(tCANMsgObject *psCANMsg, uint32_t ui32MsgObj){ unsigned int uIdx;
UARTprintf("Sending msg: obj=%d ID=0x%04X msg=0x", ui32MsgObj, psCANMsg->ui32MsgID); for(uIdx = 0; uIdx < psCANMsg->ui32MsgLen; uIdx++) { UARTprintf("%02X ", psCANMsg->pui8MsgData[uIdx]); } UARTprintf("\n");}
//*****************************************************************************//// This function provides a 1 second delay using a simple polling method.////*****************************************************************************voidSimpleDelay(void){ // // Delay cycles for 1 second // SysCtlDelay(16000000 / 3);}
//*****************************************************************************//// This function is the interrupt handler for the CAN peripheral. It checks// for the cause of the interrupt, and maintains a count of all messages that// have been transmitted.////*****************************************************************************voidCANIntHandler(void){ uint32_t ui32Status;
// // Read the CAN interrupt status to find the cause of the interrupt // ui32Status = CANIntStatus(CAN1_BASE, CAN_INT_STS_CAUSE);
// // If the cause is a controller status interrupt, then get the status // if(ui32Status == CAN_INT_INTID_STATUS) { // // Read the controller status. This will return a field of status // error bits that can indicate various errors. Error processing // is not done in this example for simplicity. Refer to the // API documentation for details about the error status bits. // The act of reading this status will clear the interrupt. If the // CAN peripheral is not connected to a CAN bus with other CAN devices // present, then errors will occur and will be indicated in the // controller status. // ui32Status = CANStatusGet(CAN1_BASE, CAN_STS_CONTROL);
// // Set a flag to indicate some errors may have occurred. // g_bErrFlag = 1; }
// // Check if the cause is message object 1, which is used for sending // message 1. // else if(ui32Status == 1) { // // Getting to this point means that the TX interrupt occurred on // message object 1, and the message TX is complete. Clear the // message object interrupt. // CANIntClear(CAN1_BASE, 1);
// // Increment a counter to keep track of how many messages have been // sent. In a real application this could be used to set flags to // indicate when a message is sent. // g_ui32Msg1Count++;
// // Since the message was sent, clear any error flags. // g_bErrFlag = 0; }
// // Check if the cause is message object 2, which is used for sending // message 2. // else if(ui32Status == 2) { // // Getting to this point means that the TX interrupt occurred on // message object 2, and the message TX is complete. Clear the // message object interrupt. // CANIntClear(CAN1_BASE, 2);
// // Increment a counter to keep track of how many messages have been // sent. In a real application this could be used to set flags to // indicate when a message is sent. // g_ui32Msg2Count++;
// // Since the message was sent, clear any error flags. // g_bErrFlag = 0; }
// // Check if the cause is message object 3, which is used for sending // messages 3 and 4. // else if(ui32Status == 3) { // // Getting to this point means that the TX interrupt occurred on // message object 3, and a message TX is complete. Clear the // message object interrupt. // CANIntClear(CAN1_BASE, 3);
// // Increment a counter to keep track of how many messages have been // sent. In a real application this could be used to set flags to // indicate when a message is sent. // g_ui32Msg3Count++;
// // Set the flag indicating that a message was sent using message // object 3. The program main loop uses this to know when to send // another message using message object 3. // g_bMsgObj3Sent = 1;
// // Since the message was sent, clear any error flags. // g_bErrFlag = 0; }
// // Otherwise, something unexpected caused the interrupt. This should // never happen. // else { // // Spurious interrupt handling can go here. // }}
//*****************************************************************************//// Configure the CAN and enter a loop to transmit periodic CAN messages.////*****************************************************************************intmain(void){ uint32_t ui32SysClock;
ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_16MHZ | SYSCTL_OSC_INT | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480), 120000000); // // Set up the serial console to use for displaying messages. This is // just for this example program and is not needed for CAN operation. // InitConsole();
// // For this example CAN1 is used with RX and TX pins on port B4 and B5. // The actual port and pins used may be different on your part, consult // the data sheet for more information. // GPIO port B needs to be enabled so these pins can be used. // TODO: change this to whichever GPIO port you are using // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
// // Configure the GPIO pin muxing to select CAN1 functions for these pins. // This step selects which alternate function is available for these pins. // This is necessary if your part supports GPIO pin function muxing. // Consult the data sheet to see which functions are allocated per pin. // TODO: change this to select the port/pin you are using // GPIOPinConfigure(GPIO_PB0_CAN1RX); GPIOPinConfigure(GPIO_PB1_CAN1TX);
// // Enable the alternate function on the GPIO pins. The above step selects // which alternate function is available. This step actually enables the // alternate function instead of GPIO for these pins. // TODO: change this to match the port/pin you are using // GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_0 | GPIO_PIN_1);
// // The GPIO port and pins have been set up for CAN. The CAN peripheral // must be enabled. // SysCtlPeripheralDisable(SYSCTL_PERIPH_CAN1); SysCtlPeripheralReset(SYSCTL_PERIPH_CAN1); SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN1);
// // Initialize the CAN controller // CANInit(CAN1_BASE);
// // Set up the bit rate for the CAN bus. This function sets up the CAN // bus timing for a nominal configuration. You can achieve more control // over the CAN bus timing by using the function CANBitTimingSet() instead // of this one, if needed. // In this example, the CAN bus is set to 500 kHz. In the function below, // the call to SysCtlClockGet() is used to determine the clock rate that // is used for clocking the CAN peripheral. This can be replaced with a // fixed value if you know the value of the system clock, saving the extra // function call. For some parts, the CAN peripheral is clocked by a fixed // 8 MHz regardless of the system clock in which case the call to // SysCtlClockGet() should be replaced with 8000000. Consult the data // sheet for more information about CAN peripheral clocking. // CANBitRateSet(CAN1_BASE, ui32SysClock, 500000);
// // Enable interrupts on the CAN peripheral. This example uses static // allocation of interrupt handlers which means the name of the handler // is in the vector table of startup code. If you want to use dynamic // allocation of the vector table, then you must also call CANIntRegister() // here. // CANIntRegister(CAN1_BASE, CANIntHandler); // if using dynamic vectors // CANIntEnable(CAN1_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
// // Enable the CAN interrupt on the processor (NVIC). // IntEnable(INT_CAN1);
// // Enable the CAN for operation. // CANEnable(CAN1_BASE);
// // Initialize the message object that will be used for sending CAN // messages. The message will be 4 bytes that will contain an incrementing // value. Initially it will be set to 0. //
// // Initialize message object 1 to be able to send CAN message 1. This // message object is not shared so it only needs to be initialized one // time, and can be used for repeatedly sending the same message ID. // g_sCANMsgObject1.ui32MsgID = 0x1001; g_sCANMsgObject1.ui32MsgIDMask = 0; g_sCANMsgObject1.ui32Flags = MSG_OBJ_TX_INT_ENABLE; g_sCANMsgObject1.ui32MsgLen = sizeof(g_pui8Msg1); g_sCANMsgObject1.pui8MsgData = g_pui8Msg1;
// // Initialize message object 2 to be able to send CAN message 2. This // message object is not shared so it only needs to be initialized one // time, and can be used for repeatedly sending the same message ID. // g_sCANMsgObject2.ui32MsgID = 0x2001; g_sCANMsgObject2.ui32MsgIDMask = 0; g_sCANMsgObject2.ui32Flags = MSG_OBJ_TX_INT_ENABLE; g_sCANMsgObject2.ui32MsgLen = sizeof(g_pui8Msg2); g_sCANMsgObject2.pui8MsgData = g_pui8Msg2;
// // Enter loop to send messages. Four messages will be sent once per // second. The contents of each message will be changed each time. // for(;;) { // // Send message 1 using CAN controller message object 1. This is // the only message sent using this message object. The // CANMessageSet() function will cause the message to be sent right // away. // PrintCANMessageInfo(&g_sCANMsgObject1, 1); CANMessageSet(CAN1_BASE, 1, &g_sCANMsgObject1, MSG_OBJ_TYPE_TX);
// // Send message 2 using CAN controller message object 2. This is // the only message sent using this message object. The // CANMessageSet() function will cause the message to be sent right // away. // PrintCANMessageInfo(&g_sCANMsgObject2, 2); CANMessageSet(CAN1_BASE, 2, &g_sCANMsgObject2, MSG_OBJ_TYPE_TX);
// // Load message object 3 with message 3. This is needs to be done each // time because message object 3 is being shared for two different // messages. // g_sCANMsgObject3.ui32MsgID = 0x3001; g_sCANMsgObject3.ui32MsgIDMask = 0; g_sCANMsgObject3.ui32Flags = MSG_OBJ_TX_INT_ENABLE; g_sCANMsgObject3.ui32MsgLen = sizeof(g_pui8Msg3); g_sCANMsgObject3.pui8MsgData = g_pui8Msg3;
// // Clear the flag that indicates that message 3 has been sent. This // flag will be set in the interrupt handler when a message has been // sent using message object 3. // g_bMsgObj3Sent = 0;
// // Now send message 3 using CAN controller message object 3. This is // the first message sent using this message object. The // CANMessageSet() function will cause the message to be sent right // away. // PrintCANMessageInfo(&g_sCANMsgObject3, 3); CANMessageSet(CAN1_BASE, 3, &g_sCANMsgObject3, MSG_OBJ_TYPE_TX);
// // Wait for the indication from the interrupt handler that message // object 3 is done, because we are re-using it for another message. // while(!g_bMsgObj3Sent) { }
// // Load message object 3 with message 4. This is needed because // message object 3 is being shared for two different messages. // g_sCANMsgObject3.ui32MsgID = 0x3002; g_sCANMsgObject3.ui32MsgIDMask = 0; g_sCANMsgObject3.ui32Flags = MSG_OBJ_TX_INT_ENABLE; g_sCANMsgObject3.ui32MsgLen = sizeof(g_pui8Msg4); g_sCANMsgObject3.pui8MsgData = g_pui8Msg4;
// // Now send message 4 using CAN controller message object 3. This is // the second message sent using this message object. The // CANMessageSet() function will cause the message to be sent right // away. //
PrintCANMessageInfo(&g_sCANMsgObject3, 3); CANMessageSet(CAN1_BASE, 3, &g_sCANMsgObject3, MSG_OBJ_TYPE_TX);
}
// // Return no errors // //return(0);}