Part Number: TM4C129ENCPDT
Hi all,
I'm trying to read analog values in multiple pins with tm4c129, but I'm getting always zero.
Can I get some help, please?
My code is attached.
/*
* adc.c
*
* Created on: 6 de set de 2017
* Author: allefpablo
*/
#include <stdarg.h>
#include <stdint.h>
#include <stdbool.h>
#include <stdio.h>
#include "inc/hw_adc.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/adc.h"
#include "driverlib/pin_map.h"
#include "board_drivers/hardware_def.h"
#include "adc.h"
static uint32_t pui32ADC0Value[11];
void adc_init()
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
//
// Select the analog ADC function for these pins.
// Consult the data sheet to see which functions are allocated per pin.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_0);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_1);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_2);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_3);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_4);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_5);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_6);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_7);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2);
//
// Enable sample sequence 3 with a processor signal trigger. Sequence 3
// will do a single sample when the processor sends a signal to start the
// conversion. Each ADC module has 4 programmable sequences, sequence 0
// to sequence 3. This example is arbitrarily using sequence 3.
//
//ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_PROCESSOR, 0);
//
// Configure step 0 on sequence 3. Sample channel 0 (ADC_CTL_CH0) in
// single-ended mode (default) and configure the interrupt flag
// (ADC_CTL_IE) to be set when the sample is done. Tell the ADC logic
// that this is the last conversion on sequence 3 (ADC_CTL_END). Sequence
// 3 has only one programmable step. Sequence 1 and 2 have 4 steps, and
// sequence 0 has 8 programmable steps. Since we are only doing a single
// conversion using sequence 3 we will only configure step 0. For more
// information on the ADC sequences and steps, reference the datasheet.
//
ADCSequenceStepConfigure(ADC0_BASE, 0, 0, ADC_CTL_CH1);
ADCSequenceStepConfigure(ADC0_BASE, 0, 1, ADC_CTL_CH2);
ADCSequenceStepConfigure(ADC0_BASE, 0, 2, ADC_CTL_CH3);
ADCSequenceStepConfigure(ADC0_BASE, 0, 3, ADC_CTL_CH4);
ADCSequenceStepConfigure(ADC0_BASE, 0, 4, ADC_CTL_CH5);
ADCSequenceStepConfigure(ADC0_BASE, 0, 5, ADC_CTL_CH6);
ADCSequenceStepConfigure(ADC0_BASE, 0, 6, ADC_CTL_CH7);
ADCSequenceStepConfigure(ADC0_BASE, 0, 7, ADC_CTL_CH12);
ADCSequenceStepConfigure(ADC0_BASE, 0, 8, ADC_CTL_CH13);
ADCSequenceStepConfigure(ADC0_BASE, 0, 9, ADC_CTL_CH14);
ADCSequenceStepConfigure(ADC0_BASE, 0, 10, ADC_CTL_CH15 | ADC_CTL_IE |
ADC_CTL_END);
IntEnable(INT_ADC0SS0);
//
// Since sample sequence 3 is now configured, it must be enabled.
//
ADCSequenceEnable(ADC0_BASE, 0);
ADCSequenceEnable(ADC0_BASE, 1);
ADCSequenceEnable(ADC0_BASE, 2);
ADCSequenceEnable(ADC0_BASE, 3);
ADCSequenceEnable(ADC0_BASE, 4);
ADCSequenceEnable(ADC0_BASE, 5);
ADCSequenceEnable(ADC0_BASE, 6);
ADCSequenceEnable(ADC0_BASE, 7);
ADCSequenceEnable(ADC0_BASE, 8);
ADCSequenceEnable(ADC0_BASE, 9);
ADCSequenceEnable(ADC0_BASE, 10);
//
// Clear the interrupt status flag. This is done to make sure the
// interrupt flag is cleared before we sample.
//
//ADCIntClear(ADC0_BASE, 0);
}
uint32_t read_adc(uint32_t sequence, uint32_t *values)
{
ADCIntClear(ADC0_BASE, sequence);
ADCProcessorTrigger(ADC0_BASE, sequence);
while(!ADCIntStatus(ADC0_BASE, sequence, false)){}
return (ADCSequenceDataGet(ADC0_BASE, sequence, values));
}
uint32_t get_voltage_ch_1()
{
return read_adc(4, pui32ADC0Value);
}
uint32_t get_voltage_ch_2()
{
return read_adc(3, pui32ADC0Value);
}
uint32_t get_voltage_ch_3()
{
return read_adc(5, pui32ADC0Value);
}
uint32_t get_voltage_ch_4()
{
return read_adc(6, pui32ADC0Value);
}
uint32_t get_current_ch_1()
{
return read_adc(2, pui32ADC0Value);
}
uint32_t get_current_ch_2()
{
return read_adc(1, pui32ADC0Value);
}
uint32_t get_current_ch_3()
{
return read_adc(0, pui32ADC0Value);
}
uint32_t get_current_ch_4()
{
return read_adc(7, pui32ADC0Value);
}
uint32_t get_lv_signal_ch_1()
{
return read_adc(8, pui32ADC0Value);
}
uint32_t get_lv_signal_ch_2()
{
return read_adc(9, pui32ADC0Value);
}
uint32_t get_lv_signal_ch_3()
{
return read_adc(10, pui32ADC0Value);
}