This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: DMA SPI TX in pingpong mode

Part Number: TM4C1294NCPDT

Tool/software: TI-RTOS

Hi,

I am using SPI TX through DMA in pingpong mode as SPI is configured as slave device.

I have configured the SPI to DMA interrupt DMA transfer complete interrupt, This interrupt will raise request if the transfer is completed.

Since I have configured the device in slave mode, it will wait for clock from master then only data will be send out of the device.

But without master clock, the interrupt is getting triggered and the ping pong is performing transfer alternately even in slave mode.

Regards,

Manohar

  • Hello Manohar,

    While your setup is presented quite well, I am not clear what your question is. Can you please clarify your concerns/questions?
  • Hi,

    My question:

    1. I have configured my SPI DMA as Slave in ping pong mode. Without the clock from master, The DMA continuous the transfer from DMA buffer to SPI buffer and not out of SPI buffer.
    I think its overwriting the SPI buffer, When I initiate a transfer from another device as master. The received data in master device is not uniform. It keep on varies.
    (E.x)Buffer data in Slave device is 1,2,3,4 . But I am receiving as 2,3,4,1.
    Don't know why this mismatch is happening.