Part Number: TMS570LS1114
Other Parts Discussed in Thread: HALCOGEN
Tool/software: TI C/C++ Compiler
Hello:
With regard to the TMS570LS1114PGE EEPROM module, I have the following questions.
1.According to the example given by HALCoGen, only the FEE module brushes the EEPROM. I looked at the Fapi document and still didn't feel like a complete example of reading and writing EEPROM. What are the difference of FAPI and FEE, and what are the applicable circumstances?
- according to document spnu501h.pdf, I need to initialize the device before I read and write. Do it specifically refer to the HaLCoGen module?
3.to achieve a fixed address, Read, Write, Erase, to achieve what operation, I have transferred the FEE module, transplantation to FAPI what is the difference?
Explanation: the function I'm trying to achieve is simply to store some important fault detection codes and a lot of calibration parameters, store them into EEPROM, and use the CCP protocol to communicate with an address datas.
Looking forward to your reply
Qiu Chi