Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hello team,
I have a question please.
I own the microcontroller TMS570LC4357 (Launchpad Development Kit). I want to capture the data of four microphones, each microphone is connected to an amplifier, and each output of the amplifier is connected to a channel in AD converter.
Is it possible to send the data from the internal ADC with the internal SPI to terminal in CCS?
If yes, what do I need to use, MIBSPI or only SPI connection?
What do I have to configure in HALCoGen?
I only have to connect the microcontroller with USB cable directly. Is it enough?
do you have a code example please?
the problem is I want to read the data from the AD converter, but with SCI is slow, or can I send my data with ethernet? Is it possible?
I would be very grateful to you for any help
Best regards
Jo