The customer has a question about GIO of R1x device (TMS470R1A288PGET).
Could you pls have a look and put your comment? Thanks.
1> what's the default status of GIOA[0] after reset? input or output, IPU or IPD?
--> according to datasheet, all I/Os are input by default, but not mention if there is internal pull up/down
2> Is external pull up/down resistor required for input mode? or just suspend?
--> I think if there is IPU/IPD, it could be suspend. pls correct me if wrong.
I am not sure above because there is no description in the datasheet for interrupt-capable pin & 5v tolerant.