Part Number: TM4C123GH6PM
I was debugging my code and restarted the code while ISR was being serviced. After reset though, the Interrupt stopped getting detected.
The problem doesn't occur if I restart my code any where in the program but happens if I reset it in the ISR.
Note: I am clearing my Interrupt at the very start of ISR.
Is this normal or is there a way to fix this problem?
My Code:
/*!
* @author Yash Bansod
* @date 19th September 2017
*
* @brief PWM Servo
* @details The program controls the position of an external servo motor by
* varying the Duty Cycle of the PWM. The Duty Cycle can be increased by
* clicking the onboard switch SW2(PF0) or decreased by clicking SW1(PF4).
* The PWM module .
* @note The tm4c123ghpm_startup_ccs.c contains the vector table for the
* microcontroller. It was modified to execute the specified ISR on
* Timer0A and PortF Interrupts.
*/
/* ----------------------- Include Files --------------------- */
#include <stdint.h> // Library of Standard Integer Types
#include <stdbool.h> // Library of Standard Boolean Types
#include "inc/tm4c123gh6pm.h" // Definitions for interrupt and register assignments on Tiva C
#include "inc/hw_memmap.h" // Macros defining the memory map of the Tiva C Series device
#include "inc/hw_types.h" // Defines common types and macros
#include "inc/hw_gpio.h" // Defines Macros for GPIO hardware
#include "inc/hw_pwm.h" // Defines and Macros for Pulse Width Modulation (PWM) ports
#include "driverlib/debug.h" // Macros for assisting debug of the driver library
#include "driverlib/pwm.h" // API function prototypes for PWM ports
#include "driverlib/sysctl.h" // Defines and macros for System Control API of DriverLib
#include "driverlib/interrupt.h" // Defines and macros for NVIC Controller API of DriverLib
#include "driverlib/gpio.h" // Defines and macros for GPIO API of DriverLib
#include "driverlib/pin_map.h" // Mapping of peripherals to pins for all parts
#include "driverlib/rom.h" // Defines and macros for ROM API of driverLib
#define PWM_FREQUENCY 50 // Define a macro for the frequency of the PWM signal in Hz
/* ----------------------- Global Variables --------------------- */
uint32_t ui32Period; // Variable to store PWM time period
volatile uint8_t ui8Adjust = 75; // Variable to store Duty Cycle of LED
/* ----------------------- Function Prototypes --------------------- */
void PortFIntHandler(void); // Prototype for ISR of GPIO PortF
/* ----------------------- Main Program --------------------- */
int main(void){
// Set the System clock to 80MHz and the PWM Module clock to 1.25 MHz
ROM_SysCtlClockSet(SYSCTL_SYSDIV_2_5 |SYSCTL_USE_PLL |SYSCTL_OSC_MAIN |SYSCTL_XTAL_16MHZ);
ROM_SysCtlPWMClockSet(SYSCTL_PWMDIV_64);
// Enable the clock for peripherals PortF and PortD and PWM1
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
// Configure the PD0 for PWM signal (PWM module 1 generator 0)
ROM_GPIOPinTypePWM(GPIO_PORTD_BASE, GPIO_PIN_0);
ROM_GPIOPinConfigure(GPIO_PD0_M1PWM0);
// Remove the Lock present on Switch SW2 (connected to PF0) and commit the change
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = GPIO_LOCK_KEY;
HWREG(GPIO_PORTF_BASE + GPIO_O_CR) |= GPIO_PIN_0;
HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0;
// Set the PF0, PF4 as Input and configure them to be Pulled-up
ROM_GPIODirModeSet(GPIO_PORTF_BASE, GPIO_PIN_4|GPIO_PIN_0, GPIO_DIR_MODE_IN);
ROM_GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_4 | GPIO_PIN_0, GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
// Configure and enable the Interrupt for PF0 and PF4
ROM_IntEnable(INT_GPIOF);
ROM_GPIOIntTypeSet(GPIO_PORTF_BASE, GPIO_PIN_4 | GPIO_PIN_0, GPIO_FALLING_EDGE);
GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_0 | GPIO_INT_PIN_4);
// Master interrupt enable API for all interrupts
ROM_IntMasterEnable();
// Calculate the Timer period of the PWM Module.
uint32_t ui32PWMClock = SysCtlClockGet() / 64;
ui32Period = (ui32PWMClock / PWM_FREQUENCY) - 1;
// Configure thE PWM1 Genrator0 to work in Count Down Mode
ROM_PWMGenConfigure(PWM1_BASE, PWM_GEN_0, PWM_GEN_MODE_DOWN);
// Load the calculated time period to the Generator0 of the PWM1 Module
ROM_PWMGenPeriodSet(PWM1_BASE, PWM_GEN_0, ui32Period);
// Set the PWM duty cycle to a specified value
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Period / 1000);
// Enable the PWM0 pin of the PWM Module 1 as output
ROM_PWMOutputState(PWM1_BASE, PWM_OUT_0_BIT, true);
// Enable the PWM Generator
ROM_PWMGenEnable(PWM1_BASE, PWM_GEN_0);
while (1);
}
/* ----------------------- Function Definition --------------------- */
void PortFIntHandler(void){
// The ISR for GPIO PortF Interrupt Handling
GPIOIntClear(GPIO_PORTF_BASE , GPIO_INT_PIN_4 | GPIO_INT_PIN_0);
// If SW1(PF4) is pressed then reduce the duty cycle
if(ROM_GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_4 | GPIO_PIN_0)== GPIO_PIN_0){
ui8Adjust--;
if (ui8Adjust < 50){
ui8Adjust = 50;
}
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Period / 1000);
}
// If SW2(PW0) is pressed then increase the duty cycle
if(ROM_GPIOPinRead(GPIO_PORTF_BASE, GPIO_PIN_4 | GPIO_PIN_0)== GPIO_PIN_4){
ui8Adjust++;
if (ui8Adjust > 100){
ui8Adjust = 100;
}
ROM_PWMPulseWidthSet(PWM1_BASE, PWM_OUT_0, ui8Adjust * ui32Period / 1000);
}
}